Hi,
Basic background information:
SDK Used: 08.06.00.42
LCD : Hantronix 18-bits, 5.7 inch, 320 x 240 resistive touch ( HDA570ST-V)
As we did not get Hantronix Driver with the SDK, we are using a close match koe-tx14d24m1bpa Driver.
Hardware Schematic:

Problem Statement:
We have an image that we are trying to display as below:

However, When it is displayed on the LCD, it looks like this.

Looks like the image is overlayed on top of other background image. The background image is similar to the default window which gets displayed when we run AM62X Starter kit.
Any help in resolving this issue would greatly appreciated.
Regards,
Swapna