This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-AM62X: AM6232 Build Options

Part Number: PROCESSOR-SDK-AM62X


Hi Team,

Below mentioned my queries.

We are building the SDK using below as mentioned in Building SDK. Command used:- MACHINE=am62xx-evm ARAGO_RT_ENABLE=1 bitbake tisdk-default-image

   Since we have AM6254 in Evaluation Board but we are going to use AM6232 in our custom Board. Is there any process we have to build the SDK only for AM6232. Can we change the MACHINE parameter in command to build SDK for particular device? Pls Confirm

Below is my Environment:

Evaluation Board:- AM62B-P1

SDK:- PROCESSOR-SDK-LINUX-RT-AM62X  Processor SDK RT-Linux for AM62x  Version: 09.00.00.03

Build Environment:- yocto build environment

Regards,

Kumar Ashutosh