Part Number: AM5728
Other Parts Discussed in Thread: BEAGLEBOARD-X15, PMP
Hi
We are not able to boot properly Custom Board based on am5728 from sd card.
we are getting Board: UNKNOWN(BeagleBoard X15?) REV UNKNOWN
U-Boot SPL 2021.01-00003-g16d964ac27-dirty (Dec 16 2023 - 20:17:00 +0530)
DRA752-GP ES2.0
U-Boot 2021.01-00003-g16d964ac27-dirty (Dec 16 2023 - 20:17:00 +0530)
CPU : DRA752-GP ES2.0
Model: TI AM5728 BeagleBoard-X15
Board: UNKNOWN(BeagleBoard X15?) REV UNKNOWN
DRAM: 2 GiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
Net: Could not get PHY for ethernet@48484000: addr 1
eth2: ethernet@48484000
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
Failed to load 'boot.scr'
347 bytes read in 10 ms (33.2 KiB/s).
i check out following forum cases but not able get proper.