Part Number: TMS320C6678
Dear TI Engineering Team
We are using a TMS320C6678 DSP in our design. We do not use the DDR memory and the signals are left open.
Voltage order is okay.
DDRCLKP is connected to +1.8V and DDRCLKN is connected to GND via a 1 kohm resistor.
DVDD15 is connected to +1.5V via a 10 ohm resistor.
We have noted that on some units DVDD15 starts at +1.5V and after 200ms it drops to +1V and after another 200ms it drops to +0.7V.
The other side of the 10ohm resistor stays at +1.5V.
Not all units behave like this. Do we have a flaw in our DSPs?
Or doesn't this voltage drop matters?
Best Regards
Lars-Olle Arnesson


Blue is DVDD15