This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM623: Usage of an eMMC boot0 partition of 4MB ?

Part Number: AM623

Hello,

The TISDK 08.06 indicates a eMMC boot partition of 8MB:

software-dl.ti.com/.../UG-Memory.html
            boot0 partition (8 MB)                        user partition
   0x0+----------------------------------+      0x0+-------------------------+
      |     tiboot3.bin (1 MB)           |         |                         |
 0x400+----------------------------------+         |                         |
      |       tispl.bin (2 MB)           |         |                         |
0x1400+----------------------------------+         |        rootfs           |
      |       u-boot.img (4 MB)          |         |                         |
0x3400+----------------------------------+         |                         |
      |      environment (128 KB)        |         |                         |
0x3500+----------------------------------+         |                         |
      |   backup environment (128 KB)    |         |                         |
0x3600+----------------------------------+         +-------------------------+

Is is possible to use an eMMC with a boot partition of 4MB ?
Which modification must be done to the SDK to handle a boot partition of 4MB ?

Could you explain if there is some risk or limitation to use such eMMC ?

Regards,

Alexis.