Part Number: AM6442
Hi, Team
The CPSW of am64x has 2 ports. From device tree and TISCI, there are 8 tx channels and 1 rx channel.
Q1: How do the two ports allocate these 8 dma sending channels?
Q2: Do the two ports use the same dma receiving channel?
Q3: Can I reset and re-initialize only a single port? Or are both ports reset at the same time? (Because there is only one mac)


Best Regards,
Zane