This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LCD display resolution changes from EBOOT do not seem to work

I am running the Logic 3517 eXperimenter Dev Kit with Compact 7 and the TI BSP (BSP 2.00.00.02). I am trying to change the resolution on the LCD in EBOOT but only the default resolution seems to work (see black screen with resolutions other than default).

Do I need to do anything other than select the resolution in EBOOT? Should all resolutions work?