Hi,
My target is C6747, with the development of CCS3.3.82.13, code generation tools v6.1.11 , Bios 5.33.06 and PSP driver (pspdrivers_01_30_00_05).
When compiling with Release option the algorithm is not stable, when compiling with Debug option the algorithm runs well.
According to above description I did some test. I switched between Release <-> Debug directory of the psp gpio by only changed the directory name (located in: C:\Program Files\Texas Instruments\pspdrivers_01_30_00_05\packages\ti\pspiom\gpio\lib\C6747) . this operation solved the problem for the Release option and caused the problem for the Debug option.
What are the differences between gpio lib in the release and debug directory (\pspdrivers_01_30_00_05\packages\ti\pspiom\gpio\lib\C6747) ?
Is it possible that my PSP version is not correct?
Where are the locations of the PSP download site?
Best regards,
Yaniv