Part Number: PROCESSOR-SDK-AM62A
Hello,
I was using SDK 9.0.1, trying to upgrade 9.1.0 using following command.
I am getting git error.
snarayanan@PG0154LT:~/yocto-build$ ./oe-layertool-setup.sh -f configs/processor-sdk-analytics/processor-sdk-analytics-09.01.00-config.txt
/home/snarayanan/yocto-build
cloning repo bitbake
Fetching origin
fatal: A branch named '2.0' already exists.
Already up to date.
HEAD is now at 42a1c9fe runqueue: show number of currently running bitbake threads when pressure changes
cloning repo meta-arago
Fetching origin
error: pathspec 'kirkstone-j722s-wakeup' did not match any file(s) known to git
merge: origin/kirkstone-j722s-wakeup - not something we can merge
ERROR: the meta-arago/meta-arago-test layer in the meta-arago repository could not be
found. Bailing out.
When i tried to do fresh install, i am getting another git error, which posted in the following thread.
1305768/processor-sdk-am62a-sdk-9-1-0-meta-arago-git-error