This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM-Q1: TDA4VM-Q1

Part Number: TDA4VM-Q1

EMMC interface, pull-up resistance 47K to 1.8V, test pull-up resistance values see the table for different resistance values, test environment: When the multimeter 15B circuit board is powered off for more than 10 hours, the test resistance of the voltmeter is equivalent to the bridge voltage output. The test resistance at both ends may cause the internal mos to open and the test resistance is abnormal, but the test resistance of other PCBA does not appear. The resistance value is basically close to 47K.why?EMMC is suspected at first, the phenomenon still exists after disassembling EMMC, but other boards are normal is TDA4 cause?

         design  A board one   A board two   A board three     B board test
CALPAD    10k       9.96K         9.96K         9.96K            9.97K 
CLK       22R       22.1R         22.1R         22.1R            22.1R
CMD       47K       9.58K         46.7K         46.7K            46.5K
DAT0      47K       9.44K         9.57K         46.6K            46.6K
DAT1      47K       9.56K         9.49K         46.7K            46.5K
DAT2      47K       9.48K         9.56K         46.5K            46.5K
DAT3      47K       9.58K         36.1K         46.7K            46.5K
DAT4      47K       9.48K         9.56K         46.8K            46.8K
DAT5      47K       9.57K         46.7K         46.7K            46.6K
DAT6      47K       46.6K         46.8K         46.5K            40.3K
DAT7      47K       46.7K         46.7K         46.6K            39.8K
DS        10K       9.65K         9.6K          9.67K            9.7K