Hi,
I'm using the TI official A8 demo, I found some problem when the wince starts. It is likely the system i2c driver don't access device infor? then the system halt,If I just need it run normal,How to do for it? thanks.
Token.
LayMgr.cpp: Layout Manager successfully initialized to 1
MSIM: IM_ReadRegistry read KB 5
Explorer(V2.0) taskbar thread started.
NDISPWR:: Found adapter [SMSC91181]
NDISPWR:: Found adapter [EMAC1]
M 132,819 130,845 -2,26M 128,846 121,867 -7,21Write: Attempts = 2
Write: Attempts = 2
Write: Attempts = 2
M 140,188 133,294 -7,106Read: Attempts = 2
Read: Attempts = 3
Read: Attempts = 4
Read: Attempts = 5
WARN: I2C: Read failed (slave addr=0x4B, register=0x00000000)
Write: Attempts = 2
Write: Attempts = 3
Write: Attempts = 4
Write: Attempts = 5
WARN: I2C: Write failed (SA=0x4B, register=0x00000000)
Write: Attempts = 2
Write: Attempts = 3
Write: Attempts = 4
Write: Attempts = 5
WARN: I2C: Write failed (SA=0x4B, register=0x00000000)