Hi,
Our customer is comparing the access speed of DDR2/DDR3 with DM814x EVM.
The below is the results of the performance.
\\\\\ Test results\\\\
Time for 1Mbytes data transfer
| Memory type | cycle number | time(msec) |
| DDR2 EVM | 4993537 | 10.0 |
| DDR3 EVM | 5452481 | 10.9 |
-test conditon-
> The measurement was done for between < DSP - DDR>
> Cache was enabled
> GEL (included in PSP) modified :
DDR 333Mhz -> 400Mhz
DMM interleave enabled
As you see the above results, DDR3 is slower than DDR2. It is approximately 10% .
I think Both of DDR2/DDR3 EVM have same performance if there are same memory clock, L3 bus speed and CPU speed.
My questions are :
1) The setting of memory latency for DDR2 EVM/DDR3 EVM seems to be different. The test of results is caused this matter?
Or are there other factor for performance down?
2) Generally speaking, clock speed of DDR3 is higher than DDR2's it. And DDR3's latency is longer than DDR2. In case of
memory using EVM, if I use lower clock than spec., is it possible that the value of latency is smaller?
Thank you for your help.
Michi