This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SK-AM62A-LP: Partial I/O wakeup sources

Part Number: SK-AM62A-LP

According to Low Power Modes - Partial I/O, mcan0 can be used for wakeup from partial I/O.

I want to use few buttons (E.g. GPIO0_38, GPIO0_39, GPIO0_40) on main_gpio0 for partial I/O.
Is it possible to use main_gpio0 for partial I/O?
If so, what are all the device tree changes has to be made?
Similar to  ethtool -s can0 wol p, what command i should give on Linux to make them as partial I/O wakeup button?

Note:
I am using Linux through YOCTO.