Part Number: AM625
Other Parts Discussed in Thread: AM623, , AM620-Q1
Hi, TI community,
We are using AM625 on our custom board and I have a question about the mmc2.
We tried connecting MMC2 to SD card or eMMC, I modified the DTSI settings to align the configuration of MMC2 with that of MMC0 or MMC1.
but both failed, and I printed the error log as below
"mmc2: req failed (CMD5): -110, retrying..."
I checked "AM62x Sitara Processors", MMCSD part, seems only MMC0 supports eMMC, is that right?
But I tried to modify sdhci2 as same as sdhci1 still failed.
Is there anything I missed?
Dtsi setting : sdhci1: mmc@fa00000 {
compatible = "ti,am62-sdhci";
reg = <0x00 0x0fa00000 0x00 0x1000>, <0x00 0x0fa08000 0x00 0x400>;
interrupts = <GIC_SPI 83 IRQ_TYPE_LEVEL_HIGH>;
power-domains = <&k3_pds 58 TI_SCI_PD_EXCLUSIVE>;
clocks = <&k3_clks 58 5>, <&k3_clks 58 6>;
clock-names = "clk_ahb", "clk_xin";
ti,trm-icp = <0x2>;
ti,otap-del-sel-legacy = <0x8>;
ti,otap-del-sel-sd-hs = <0x0>;
ti,otap-del-sel-sdr12 = <0x0>;
ti,otap-del-sel-sdr25 = <0x0>;
ti,otap-del-sel-sdr50 = <0x8>;
ti,otap-del-sel-sdr104 = <0x7>;
ti,otap-del-sel-ddr50 = <0x4>;
ti,itap-del-sel-legacy = <0xa>;
ti,itap-del-sel-sd-hs = <0x1>;
ti,itap-del-sel-sdr12 = <0xa>;
ti,itap-del-sel-sdr25 = <0x1>;
ti,clkbuf-sel = <0x7>;
bus-width = <4>;
status = "disabled";
};
sdhci2: mmc@fa20000 {
compatible = "ti,am62-sdhci";
reg = <0x00 0x0fa20000 0x00 0x1000>, <0x00 0x0fa28000 0x00 0x400>;
interrupts = <GIC_SPI 82 IRQ_TYPE_LEVEL_HIGH>;
power-domains = <&k3_pds 184 TI_SCI_PD_EXCLUSIVE>;
clocks = <&k3_clks 184 5>, <&k3_clks 184 6>;
clock-names = "clk_ahb", "clk_xin";
ti,trm-icp = <0x2>;
ti,otap-del-sel-legacy = <0x8>;
ti,otap-del-sel-sd-hs = <0x0>;
ti,otap-del-sel-sdr12 = <0x0>;
ti,otap-del-sel-sdr25 = <0x0>;
ti,otap-del-sel-sdr50 = <0x8>;
ti,otap-del-sel-sdr104 = <0x7>;
ti,otap-del-sel-ddr50 = <0x4>;
ti,itap-del-sel-legacy = <0xa>;
ti,itap-del-sel-sd-hs = <0x1>;
ti,itap-del-sel-sdr12 = <0xa>;
ti,itap-del-sel-sdr25 = <0x1>;
ti,clkbuf-sel = <0x7>;
bus-width = <4>;
status = "disabled";
};
&sdhci1 {
/* SD card */
vmmc-supply = <&vcc_3v3_sys>;
vqmmc-supply = <&vcc_3v3_sys>;
pinctrl-names = "default";
pinctrl-0 = <&main_mmc1_pins_default>;
ti,driver-strength-ohm = <50>;
disable-wp;
sdhci-caps-mask = <0x00000006 0x00000000>; /* Limiting to DDR50 speed mode */
ti,fails-without-test-cd;
};
&sdhci2 {
status = "okay";
bus-width = <4>;
/* DiskA card */
vmmc-supply = <&vcc_3v3_sys>;
vqmmc-supply = <&vcc_3v3_sys>;
pinctrl-names = "default";
pinctrl-0 = <&main_mmc2_pins_default>;
ti,driver-strength-ohm = <50>;
disable-wp;
sdhci-caps-mask = <0x00000006 0x00000000>; /* Limiting to DDR50 speed mode */
ti,fails-without-test-cd;
};main_mmc1_pins_default: main-mmc1-pins-default {
pinctrl-single,pins = <
AM62X_IOPAD(0x23c, PIN_INPUT, 0) /* (A21/C18) MMC1_CMD */
AM62X_IOPAD(0x234, PIN_INPUT, 0) /* (B22/A20) MMC1_CLK */
AM62X_IOPAD(0x230, PIN_INPUT, 0) /* (A22/A19) MMC1_DAT0 */
AM62X_IOPAD(0x22c, PIN_INPUT, 0) /* (B21/B19) MMC1_DAT1 */
AM62X_IOPAD(0x228, PIN_INPUT, 0) /* (C21/B20) MMC1_DAT2 */
AM62X_IOPAD(0x224, PIN_INPUT, 0) /* (D22/C19) MMC1_DAT3 */
AM62X_IOPAD(0x240, PIN_INPUT, 0) /* (D17/C15) MMC1_SDCD */
>;
};
main_mmc2_pins_default: main-mmc2-pins-default {
pinctrl-single,pins = <
AM62X_IOPAD(0x120, PIN_INPUT, 0) /* (C24) MMC2_CMD */
AM62X_IOPAD(0x118, PIN_INPUT, 0) /* (D25) MMC2_CLK */
AM62X_IOPAD(0x114, PIN_INPUT, 0) /* (B24) MMC2_DAT0 */
AM62X_IOPAD(0x110, PIN_INPUT, 0) /* (C25) MMC2_DAT1 */
AM62X_IOPAD(0x10c, PIN_INPUT, 0) /* (E23) MMC2_DAT2 */
AM62X_IOPAD(0x108, PIN_INPUT, 0) /* (D24) MMC2_DAT3 */
AM62X_IOPAD(0x124, PIN_INPUT, 0) /* (A23) MMC2_SDCD */
>;
};
Thanks,
Allen