This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5718: Ethernet loopback test with emulator

Part Number: AM5718


Hello,

I am struggling to perform a Ethernet PHY loop back test using an emulator with the Sitara.

I succeed to access the PHY through MDIO (I can read the ID register for example). The Ethernet is working correctly with operating SW.

We use a PHY connected on RMII1 (ie port 2 on Sitara).

When the test is performed, the CPDMA_STATERAM TX channel 0 completion pointer register is updated to the descriptor, and "TX descriptor word 3" is updated by Sitara from "0xE4120130" to "0xD4120130", indicating the packet has been transfered.

But "STATS GOOD_TX_FRAMES" is still at 0x0, and nothing can be observed on rmii1_txd0, rmii1_txd1 and rmii1_txen signals between Sitara and PHY using an oscilloscope. 

 Note: when CPSW_CONTROL is configured in loop back mode, I receive the frame correctly and the RX0 completion pointer iand RX descriptor word 3" are updated correctly.

Sitara AM5718, Ethernet PHY loop back test (RMII link)

Clock configuration from external 50MHz:
 @0x4a0093d0 set to 0x09000002      : CM_GMAC_GMAC_CLKCTRL[27:24]/CLKSEL_RFT/CLKSEL_REF, source of the GMAC_RFT_CLK: L3_ICLK, source of the RMII_50MHZ_CLK functional clock: GMAC_RMII_CLK ; [1:0]/ MODULEMODE, Module is explicitly enabled.
 @0x4a0093d0 set to 0x09000002      : CM_GMAC_GMAC_CLKCTRL[27:24]/CLKSEL_RFT/CLKSEL_REF, source of the GMAC_RFT_CLK: L3_ICLK, source of the RMII_50MHZ_CLK functional clock: GMAC_RMII_CLK ; [1:0]/ MODULEMODE, Module is explicitly enabled.
 @0x4A003C14 set to 0x00000100      : CTRL_CORE_SMA_SW_6: bit 8=0x100= enable 50MHz input clock for Ethernet

Pin mux configuration for RMII1:
 @0x4A003650 set to 0x00050102      : ball W9, CTRL_CORE_PAD_RGMII0_TXC rmii1_rxd1
 @0x4A003654 set to 0x00050102      : ball V9, CTRL_CORE_PAD_RGMII0_TXCTL rmii1_rxd0
 @0x4A003670 set to 0x00030002      : ball V4, CTRL_CORE_PAD_RGMII0_RXD3 rmii1_txd0
 @0x4A00366C set to 0x00010002      : ball V5, CTRL_CORE_PAD_RGMII0_RXCTL rmii1_txd1
 @0x4A00364C set to 0x00050102      : ball Y1, CTRL_CORE_PAD_UART3_TXD rmii1_rxer
 @0x4A003648 set to 0x00050102      : ball V2, CTRL_CORE_PAD_UART3_RXD rmii1_crs
 @0x4A003668 set to 0x00050002      : ball U5, CTRL_CORE_PAD_RGMII0_RXC :rmii1_txen

RMII mode selection:
 @0x4A002554 set to 0x3311 			: CTRL_CORE_CONTROL_IO_1: RMII for RMII0 (port 1) and RMII1 (port 2= PHY)

Clocks:
 @0x4A0093C0 set to 0x00000000		: CM_GMAC_CLKSTCTRL: CLKSEL_RFT=no sleep
 @0x4A0093D0 set to 0x09000002		: CM_GMAC_GMAC_CLKCTRL: Module is enabled with ext 50MHz clock
 @0x4A003644 set to 0x0004000F		: CTRL_CORE_PAD_RMII_MHZ_50_CLK: 50MHz Sitara input on GPIO5_17, output off

Apply Soft Reset to GMAC_SW Subsystem, CPSW_3G, CPGMAC_SL1/2, and CPDMA:
 @0x48484008 set to 0x00000001      :  CPSW_SOFT_RESET - GMAC_SW 3G logic (INT, REGS, CPPI, and SPF modules) reset
 Wait
 @0x48484D8C set to 0x00000001      :  SL_SOFT_RESET SL1
 Wait
 @0x48484DCC set to 0x00000001      :  SL_SOFT_RESET SL2
 Wait
 @0x4848481C set to 0x00000000      :  CPDMA_SOFT_RESET
 Wait
 @0x48485204 set to 0x00000001      :  WR_SOFT_RESET
 Wait

Initialize the HDPs (Header Description Pointer) and CPs (Completion Pointer) to NULL
 @0x48484A00--0x48484A7F set to 0x00000000    :  Clear buffer descriptor pointer CPDMA_RX*/TX*_HDP and CPDMA_RX*/TX*_CP
Interrupt setting: 
 @0x4848488C set to 0x000000FF      :  CPDMA_TX_INTMASK_CLEAR: TX interrupts disabled
 @0x484848AC set to 0x0000FFFF      :  CPDMA_RX_INTMASK_CLEAR: TX interrupts disabled
 @0x484848BC set to 0x00000003      :  CPDMA_DMA_INTMASK_CLEAR: interrupts disabled
 @0x48484888 set to 0x00000003      :  CPDMA_INT TX interrupt mask set register: 
CPSW (=SS: Port 0=Sitara/1=VAHM_switch/2=PHY) switch setting:
 @0x48484004 set to 0x00000000 		: CPSW_CONTROL (Switch control register) 0x0 as reset, no Fifo loopback
 @0x4848400C set to 0x00000007 		: CPSW_STAT_PORT_EN: statistics enabled for Ports 0,1,2
 @0x48484024 set to 0x00000007		: CPSW_FLOW_CONTROL: enable for Ports 0&1&2
Configure the ALE (Address Lookup Engine): (autorise addresses et multicast)
 @0x48484D08 set to 0x80000014 		: (TBD: ok 0x80000014, KO 0x80000110) ALE_CONTROL: enable, bypass Address Lookup Engine, Flood if VLAN not found 
 @0x48484D40 set to 0xFFFF0003 		: ALE_PORTCTL0: port 0 forward
 @0x48484D44 set to 0xFFFF0003 		: (TBD: ok 0xFFFF0000, KO 0xFFFF0003) ALE_PORTCTL1: port 1 forward 
 @0x48484D48 set to 0xFFFF0003 		: (TBD: ok 0xFFFF0000, KO 0xFFFF0003) ALE_PORTCTL2: port 2 forward (TBD: autoriser pour envoyer sur port 2? => FFFF0003)
Configure the MDIO (already done)
Configure the CPDMA:
 @0x48484804 set to 0x00000001      :  Configure the CPDMA transmit DMA controller: Tx enable
 @0x48484814 set to 0x00000001      :  Configure the CPDMA receive DMA controller: Tx enable
 @0x48484820 set to 0x00000010      :  CPDMA DMACONTROL: RX error frames transferred
Configure the CPPI TX and RX Descriptors ($24.11.4.11):
 @&RX_buffer_descriptor+0x0 set to 0x00000000  :  Configure the CPPI RX Data word 0 : next descriptor pointer 
 @&RX_buffer_descriptor+0x4 set to &RX_buffer  :  Configure the CPPI RX Data word 1 : buffer pointer
 @&RX_buffer_descriptor+0x8 set to 0x000001EF  :  Configure the CPPI RX Data word 2 : buffer offset, buffer length
 @&RX_buffer_descriptor+0xC set to 0x20020000  :  Configure the CPPI RX Data word 3 : start, from port 2=RMII1
 @&TX_buffer_descriptor+0x0 set to 0x00000000  :  Configure the CPPI TX Data word 0 : next descriptor pointer 
 @&TX_buffer_descriptor+0x4 set to &TX_buffer  :  Configure the CPPI TX Data word 1 : buffer pointer 
 @&TX_buffer_descriptor+0x8 set to 0x00080130  :  Configure the CPPI TX Data word 2 : buffer offset (+8 = skip preamble), buffer length (0x130 = wo preamble, with CRC)
 @&TX_buffer_descriptor+0xC set to 0xE4120130  :  Configure the CPPI TX Data word 3 : packet start/end, CRC in packet, to port 2, length (0x130 with CRC) ... 
 @0x01E23100 set to 0x51E02020      :  MAC-RXMBPENABLE - Receive Multicast/Broadcast/Promiscuous Channel Enabled to Rx0
Configure sliver CPGMAC_SL1 and CPGMAC_SL2, as per the desired mode of operations
 @0x48484D84 set to 0x01E00039      :  SL1_MACCONTROL - RMII, 10MB/s, Full duplex, no loopback
 @0x48484DC4 set to 0x01E00039      :  SL2_MACCONTROL - RMII, 10MB/s, Full duplex, no loopback
PORT setting:
 @0x48484100 set to 0x01300000 		: CPSW_3GF PORT 0 control register (0x01300000: no priority, VLAN LTYPE 1&2 enabled)
 @0x48484200 set to 0x01300000 		: CPSW_3GF PORT 1 control register (0x01000000: no priority)
 @0x48484300 set to 0x01300000 		: CPSW_3GF PORT 2 control register (0x00000000: priority effect)
 @0x48484220 set to 0x000001FF      :  P1_SA_HI: port 1 MAC source address low
 @0x48484224 set to 0xECADEFBA      :  P1_SA_HI: port 1 MAC source address high 
 @0x48484320 set to 0x000000FF      :  P2_SA_HI: port 2 MAC source address low 
 @0x48484324 set to 0xECADEFBA      :  P2_SA_HI: port 2 MAC source address high 
SPF = Static Packet Filter: disabled
CPTS = Time Sync : Disabled
WR = wrapper (interruptions)
 @0x48485208 set to 0x00000005      :  Wrapper, Subsystem control register: no idle
Start up RX and TX DMA:
 @0x48484A20 set to &RX_buffer_descriptor  :  RX0_HDP - buffer descriptor pointer. Start up RX DMA (Write to HDP of RX)
 Wait
 @0x48484A00 set to &TX_buffer_descriptor  :  TX0_HDP - buffer descriptor pointer. Start up TX DMA (Write to HDP of TX)
 Wait

*****************************************************************
Registers value after that is:
 CM_GMAC_CLKSTCTRL      @0x4A0093C0 = 0x00001F00 => clock running, no idle => ok
 CM_GMAC_GMAC_CLKCTRL   @0x4A0093D0 = 0x09000002 => enabled, GMAC_RMII_CLK (ext pin) used => ok
 CTRL_CORE_PAD_RMII_MHZ_50_CLK @0x4A003644 = 0x0005000F => input enable, Pull up, driver off
 CTRL_CORE_SMA_SW_6     @0x4A003C14 = 0x00000100 => ext clock from pin
 CTRL_CORE_CONTROL_IO_1 @0x4A002554 = 0x00003311
 CPSW_SOFT_IDLE         @0x48484014 = 0x00000000
 PDMA_DMASTATUS         @0x48484824 = 0x80000000 => idle
 SL1_MACSTATUS          @0x48484D88 = 0x80000000 => idle
 SL2_MACSTATUS          @0x48484DC8 = 0x80000000 => idle
 WR_STATUS              @0x4848528C = 0x00000006 => SPF1&2 (Static Packet Filter) disabled. 
 STATS GOOD_TX_FRAMES   @0x48484934 = 0x00000000 => KO (all STATS registers are at 0)
 STATS TX_OCTETS        @0x48484964 = 0x00000000
 STATS GOOD_RX_FRAMES   @0x48484900 = 0x00000000
 TX0_CP                 @0x48484A40 = 0x48486000 => ok (CPDMA_STATERAM TX channel 0 completion pointer register updated
 TX0_HDP                @0x48484A00 = 0x00000000 => ok (CPDMA_STATERAM TX channel 0 head descriptor pointer updated
 TX descriptor word 3   @0x4848600C = 0xD4120130 => ok, paquet envoyé (écrit 0xE4120130 => 0xF4120130 à tester?)
 RX0_CP                 @0x48484A60 = 0x00000000 => KO (CPDMA_STATERAM RX channel 0 completion pointer register)
 RX descriptor word 2   @0x48486008 = 0x000001EF
 RX descriptor word 3   @0x4848620C = 0x20020000

I don't know what is wrong in my initialisation (please see embedded configuration and result file).

Thanks for your return,

  Benoît