Hi,
My customer would like to confirm about the frequency on OSPI tap mode. Could you please answer their questions below.
Q1: Can the PHY mode not be used if SDR 8S-8S-8S is used ?
It seems like the driver is configured that way.
Q2: The customer believes that tap mode is activated when PHY mode is disabled (OSPI_CONFIG_REG Register bit3 = 0). Are they correct?
Q3: If Q2 is yes, is it impossible to achieve 50MHz or higher with SDR in tap mode?
(Actually, with PHY mode disabled, 100MHz can be set and it seems to be working.)
Is it prohibited by some reason ? Actually, it can work at >50MHz on SDR.
They’re asking you above question by referring Chapter 7.10.5.14 OSPI in the datasheet.
From the description in this Chapter, the software support is still needed in order to achieve DDR due to Errata. .Instead it looks like it's finally possible.to achieve with SDR 100MHz.
Thanks and regards,
Hideaki