Can TI Sitara/Integra/Davinci support multiple displays simultaneously? If so, how many?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Just to summarize.
HDVPSS has 3 independent pixels clocks. So it can support 2 independent HD displays and 1 independent SD display. For third display clock has to be derived for any of the two HD displays. Further 3 independent video contents(YUV) can be rendered and 3 independent graphics content(RGB) can be rendered on any of the available displays. Out of 3 independent video contents 1 is SD and other 2 can be HD/SD. Composition is also available between graphics and video contents on all displays.
Regards,
Hardik Shah