Part Number: SK-AM62A-LP
Hello Champs,
Customer is using the SDK \examples\drivers\boot\sbl_sd project generated tiboot3.bin file and copy to SD card BOOT part,set boot switch 01000000 11000010 SD card mode, power on, but the UART not output anything, is it related to the HS-FS type? do you know how to fix this?
BTW, when he used inux sdk pre-build tiboot3.bin, it can boot successfully from sd card. Is it a bug in MCU SDK?
Borad: AM62A-LP HS-FS EVM
MCU SDK :mcu_plus_sdk_am62ax_09_00_00_19
Project: mcu_plus_sdk_am62ax_09_00_00_19\examples\drivers\boot\sbl_sd
Thanks
Regards
Shine