Part Number: AM623
Other Parts Discussed in Thread: SK-AM62
Hello TI
The version of SDK I use:ti-processor-sdk-linux-rt-am62xx-evm-08.06.00.42.
Using the CPU model of HS-FS, it is found that the CPU startup process into uboot will fail probabilistically, and the probability of the problem is 1%.
The following screenshot shows the error:

I hope you can help me.