hi TI expert,
I receive four sets of data from Aournd camera in a cycle, i use vxSwapImageHandle to reliaze zero memcpy.
vxSwapImageHandle(yuv_image_f, camj_data, NULL, nplanes1); //front camera
vxSwapImageHandle(yuv_image_b, camj_data, NULL, nplanes1); //back camera
vxSwapImageHandle(yuv_image_l, camj_data, NULL, nplanes1); //left camera
vxSwapImageHandle(yuv_image_r, camj_data, NULL, nplanes1); //right camera
then I can use yuv_image_* without memcpy. Now I want to use mosaic node to Mosaic a picture, but the sixth parameter is a object array, how can i convert yuv_image_* to a object array in order to use mosic node?
VX_API_ENTRY vx_node VX_API_CALL tivxImgMosaicNode(vx_graph graph,
vx_kernel kernel,
vx_user_data_object config,
vx_image output_image,
vx_image background_image,
vx_object_array input_arr[],
vx_uint32 num_inputs)