Dears,
I'm using Beagleboard rev C4 and try to configure usb Ethernet external device. So I enabled Davincom DM9601 based usb, and after that I had a 3.2 MB uImage.
Unfortunately, when booting, beagleboard stops at "starting kernel", do nothing. Moreover, I have the same problem when trying to enable USB gadget Ethernet , which also generated 3.2 Mb uImage.
Here is my log:
Beagle Rev C4
Starting X-loader on MMC
tarting OS Bootloader from MMC...
Starting OS BootloadeRAM: 256 MiB
NAND: HW ECC [Kernel/FS layout] selected
256 MiB
In: serial
Out: serial
Err: serial
Beagle Rev C4
boot: 5 mmc1 is available
## Executing script at 82000000
reading uImage
k0p1/uImage *****
## Booting kernel from Legacy Image at 81000000 ...
Image Name: Linux-2.6.37-g06ebbba-dirty
Image Type: ARM Linux Ke416 Bytes = 3.2 MiB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel...
Any one know how to solve this situation? Thanks