This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Sir,
I am bringing up the camera with Deserializer DS90UB964-Q1EVM.
When I am connecting the 4meter FPD Link cable (in-vehicle) with the camera to TDA4EVM, the camera does not get up, whereas in the same environment when I plug the camera with a 10cm FPD Link cable it gets up.
Can you please let me know, if this Deserializer is tested with a 4-meter FPD Link cable?
Camera Resolution : 1280x944
Thanks and Regards,
Vyom Mishra
Hi Vyom,
The DS90UB964 operation in regard to cable length is determined by channel specification performance for insertion and return loss. We have seen typical cable reaches of 10-15m. With low loss cables, the reach of the cable will be extended whereas, high loss cables may only see success in shorter cables.
Would you be able to provide insight on the cable type being used? Additionally, what serializer is being used? Is the serializer a custom solution?
Best,
Zoe
Hello Zoe,
Thanks for the response.
We are using
Rosenberger FAKRA connectors 4meter length
Sensor: ISX016 (Serializer DS90UB913xx)
Thanks and Regards,
Vyom Mishra
Hi Vyom,
From the initial post, it was stated the camera is brought up successfully with the shorter length cable. What is the lock status on the DS90UB964? This can be read by register 0x4D for each port.
Additionally, would you be able to share the Margin Analysis results for the DS90UB964 in a good and bad case?
Best,
Zoe
Dear Zoe,
I have tried to dump the value of 0x4D, but getting some garbage value.
Regarding the margin analysis, we will plan that soon and share the results with you.
Thanks and Regards,
Vyom Mishra
Hi Vyom,
Thanks for the update! Let me know once you get these results.
Best,
Zoe
Dear Zoe,
Thanks for the support and responses.
We have successfully resolved all issues and all 4-cameras are working with 4-meter length cables.
Thanks and Regards,
Vyom Mishra