SA
-We are using 2 C6455 kits one as a transmitter & the other as a receiver
The transmitter one: we send constant digital samples for example=ones here's the part of the code:
for (i = 0; i < BUFFSIZE_tx; i++)
{
outbuf[i] =1;
}
the outbuf samples are converted via the DAC to analog signal & are transmitted to the receiver kit via an audio cable.
@The receiver kit: These analog signal is converted to digital again via the ADC
Now,we want to see these digital samples & Compare with ones signal,how we can see these received digital signal?
Can we see these received samples by inserting break point & 'Add watch expression' or not?
Thanks alot