This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SK-AM62A-LP: Compile C files using aarch64-oe-linux-gcc

Part Number: SK-AM62A-LP

Hi Ti Team,

  

I want to compile .C files using aarch64-oe-linux-gcc,but now there are many link errors when compiling.

I tried to solve it by searching the blog, but it still remains unsolved. Can you help me?

Best Regards,

Ruihua

  • I want to compile .C files using aarch64-oe-linux-gcc,but now there are many link errors when compiling.

    If you want to use the compiler directly you'll need to specify the proper sysroot using the --sysroot parameter. However it's easier to just source the provided cross-compile ENV script which will take care of this for you, like this:

    a0797059@dasso:~/ti/ti-processor-sdk-linux-edgeai-am62axx-evm-09_01_00_07/linux-devkit
    $ source environment-setup
    [linux-devkit]:~/ti/ti-processor-sdk-linux-edgeai-am62axx-evm-09_01_00_07/linux-devkit> cat << EOF > helloworld.c
    > #include <stdio.h>
    
    int main() {
        printf ("Hello World from TI!!!\n");
        return 0;
    }
    > EOF
    [linux-devkit]:~/ti/ti-processor-sdk-linux-edgeai-am62axx-evm-09_01_00_07/linux-devkit> cat helloworld.c
    #include <stdio.h>
    
    int main() {
        printf ("Hello World from TI!!!\n");
        return 0;
    }
    [linux-devkit]:~/ti/ti-processor-sdk-linux-edgeai-am62axx-evm-09_01_00_07/linux-devkit> $CC helloworld.c -o helloworld
    [linux-devkit]:~/ti/ti-processor-sdk-linux-edgeai-am62axx-evm-09_01_00_07/linux-devkit> file helloworld
    helloworld: ELF 64-bit LSB executable, ARM aarch64, version 1 (SYSV), dynamically linked, interpreter /lib/ld-linux-aarch64.so.1, BuildID[sha1]=d692d61d922a4ab3f47e32a28561740efaf64694, for GNU/Linux 3.14.0, with debug_info, not stripped

    The respective documentation regarding this can be found here: https://software-dl.ti.com/processor-sdk-linux/esd/AM62AX/09_01_00/exports/docs/linux/Overview/GCC_ToolChain.html#linux-devkit

    Regards, Andreas