Part Number: TMDSEVM572X
Can I connect USB extension card instead of display for audio signal transmission and reception?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMDSEVM572X
Can I connect USB extension card instead of display for audio signal transmission and reception?
Hello Rathna,
Yes, theoretically this should be doable. It is difficult to say any more without digging into the details. Technically you could connect any USB 2.0 or USB 3.0 complaint device. there is also on-board audio in and out for a 3,5 mm jack as seen in the User's guide.

Best
-Jouse