Other Parts Discussed in Thread: CCSTUDIO, TMS320C6670
Hello,
I have the same problem that Joseph have; setup is as followed:
-TMDXEVM6678L-Board is used
-Installed CCS Version 5.1.0.07001
-StartUp-Guide worked fine with HUA
-Following the steps in BiosMulticoreSDK_2.0_GettingStartedGuide.pdf until the Target-Connection
I've checked everything mentioned in this thread -> everyting is fine. While connection to the core, the following
error occurs:
IcePick_D: Error connecting to the target: (Error -2131 @ 0x0) Unable to access device register. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 5.0.470.0)
Can somebody help?
Best Regards,
Bernd