This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5728: Regarding accessing USB data in AM5728 eval board

Part Number: AM5728

Hi,
I recently purchased a AM5728 eval board https://www.ti.com/tool/TMDSEVM572X and sdk i am using is version 4.00 my board has 3 usb ports and i have a temp sensor when connected to a normal PC using USB i am able to see temp sensor data using screen /dev/ttyUSB0 115200 and i want to do the same the same in my AM5728 board but i am not able to see any ttyUSB once i connect my temp sensor to any one of the USB ports in eval board. It shows high speed USB device connected and when i go to /dev i am not able to regonize which is my device when is use lsusb command in AM5728 i am able to see the device connected i am able to see its bus ide and everything even  using dmesg command it  shows ony high spped USB cinnected not its TTY port . I want to see its data as i see in my linux PC any idea on any specific configuration to be done in AM5728 if any would help it would be helpful.

Regards,
Suriya