Other Parts Discussed in Thread: SYSCONFIG
Dear Experts,
I am attempting to modify the DTS file located at .../arch/arm/boot/dts/xxx.dtsi. In the file, there is a section of code as follows:
emmc_pins_default: emmc-default-pins {
pinctrl-single, pins = <
AM62X_IOPAD(0X0220, PIN_INPUT, 0) /* (Y3) MMC0_CMD */
...
...
AM62X_IOPAD(0X0204, PIN_INPUT, 0) /* (AB2) MMC0_DAT4*/
>;
};
So here,
Q1. What is the naming convention of AM62X_IOPAD, 0x0220, PIN_INPUT, and the value 0?
Q2. Where can I find the proper documentation about them?
Q3. What is the relation between "0X0204", "PIN_INPUT", and "0" as these pin attributes?
Thank you very much for your help in advance
Best Regards,
Ravikumar