Hi
I have a dm355 board and I want to run the demos. I am also using ridgerun sdk. I run make config in /home/user/DM355SDK folder and in the proprietary software option, I checked DVSDK codec demos and run make to build the file system. Now when I see the file system, there is no folder "/opt/dvsdk" but there is a folder "/opt/dvsdk_demos". When I manually copy dvsdk folder, it disagrees about kernel version. So where do I have to change the config somewhere else so that it copies folder /opt/dvsdk. ?