This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to program the 5505 USB stick FLASH with an application?

I'm new to the ezDSP 5505 platform. Just finished watching the introductory videos, which were great.

I followed every step of the "create a new project" video and it worked perfectly. Apparently the "load program" command run from CCS debugger loads the application into RAM. So, after the debug session is over, the code is lost.

How can a new application be loaded into FLASH, so that it runs on the stick when it's powered but not connected to CCS?

If this is complicated, it could be a good topic for a 3rd video.