Part Number: SK-AM62A-LP
Other Parts Discussed in Thread: AM62A7, SK-AM62B-P1, , SK-AM64B, SYSCONFIG
Hi Sir,
We are facing problem with boot up EVM.
We have downloaded file and create MicroSD card image through Quick Start Guide, but the UART log did not allow me to enter "root".
There are 3 different logs:
Log 1:
[ 218.276979] rcu: INFO: rcu_preempt detected expedited stalls on CPUs/tasks: { 0-.... } 52881 jiffies s: 93 root: 0x1/.
[ 218.287696] rcu: blocking rcu_node structures (internal RCU debug):
[ 218.293961] Task dump for CPU 0:
[ 218.297190] task:swapper/0 state:R running task stack:0 pid:0 ppid:0 flags:0x0000000a
[ 218.307101] Call trace:
[ 218.309548] __switch_to+0xd4/0x130
[ 218.313049] 0xffee280c
[ *** ] A start job is running for D-Bus Sy# Message Bus (3min 35s / 4min 33s)
[ ***] A start job is running for D-Bus Sy# Message Bus (3min 35s / 4min 33s)
Log 2:
[ OK ] Reached target Basic System.
[ 27.645029] rcu: INFO: rcu_preempt self-detected stall on CPU
[ 27.650781] rcu: 0-....: (5249 ticks this GP) idle=433c/1/0x4000000000000000 softirq=1387/1393 fqs=2602
[ 27.660247] (t=5253 jiffies g=345 q=23085 ncpus=4)
[ 27.665117] CPU: 0 PID: 227 Comm: systemd-udevd Tainted: G O 6.1.46-g247b2535b2 #1
[ 27.674058] Hardware name: Texas Instruments AM62A7 SK (DT)
[ 27.679615] pstate: 40000005 (nZcv daif -PAN -UAO -TCO -DIT -SSBS BTYPE=--)
[ 27.686561] pc : _stext+0xa4/0x2a4
[ 27.689961] lr : _stext+0x6c/0x2a4
[ 27.693353] sp : ffff800008003f60
[ 27.696656] x29: ffff800008003f60 x28: ffff000801788000 x27: 0000000000000280
[ 27.703782] x26: 0000000000000000 x25: 0000000000000000 x24: ffff8000090bd000
[ 27.710906] x23: 0000000060000005 x22: ffff8000090c3000 x21: ffff8000090bd9c8
[ 27.718031] x20: ffff8000092260c0 x19: ffff000801788000 x18: 0000000000000000
[ 27.725156] x17: ffff800876775000 x16: ffff800008000000 x15: 00009875fe97ce38
[ 27.732280] x14: 0000000000000312 x13: 0000000000000001 x12: 0000000000000000
[ 27.739404] x11: ffff00087f8391c0 x10: ffff80000923fcb0 x9 : ffff800009229d38
[ 27.746528] x8 : 000000018091b500 x7 : 7fffffffffffffff x6 : 00000000462690a3
[ 27.753652] x5 : 03ffffffffffffff x4 : 0000000000000015 x3 : ffff000801788000
[ 27.760777] x2 : ffff800876775000 x1 : 00000000000000e0 x0 : ffff8000090c3b00
[ 27.767902] Call trace:
[ 27.770338] _stext+0xa4/0x2a4
[ 27.773384] ____do_softirq+0x10/0x20
[ 27.777038] call_on_irq_stack+0x24/0x4c
[ 27.780952] do_softirq_own_stack+0x1c/0x30
[ 27.785125] __irq_exit_rcu+0xcc/0xf4
[ 27.788778] irq_exit_rcu+0x10/0x20
[ 27.792258] el1_interrupt+0x38/0x70
[ 27.795829] el1h_64_irq_handler+0x18/0x2c
[ 27.799914] el1h_64_irq+0x64/0x68
[ 27.803306] finish_task_switch.isra.0+0x80/0x230
[ 27.808002] __schedule+0x234/0x664
[ 27.811483] schedule+0x5c/0xcc
[ 27.814616] do_nanosleep.constprop.0+0x5c/0x160
[ 27.819226] hrtimer_nanosleep+0xa0/0x120
[ 27.823228] common_nsleep+0x44/0x70
[ 27.826797] __arm64_sys_clock_nanosleep+0xcc/0x150
[ 27.831663] invoke_syscall+0x48/0x114
[ 27.835404] el0_svc_common.constprop.0+0xd4/0xfc
[ 27.840098] do_el0_svc+0x20/0x30
[ 27.843405] el0_svc+0x28/0xa0
[ 27.846453] el0t_64_sync_handler+0xbc/0x140
[ 27.850712] el0t_64_sync+0x18c/0x190
[ 27.854378] rcu: INFO: rcu_preempt detected expedited stalls on CPUs/tasks: { 0-.... } 5287 jiffies s: 113 root: 0x1/.
[ 27.865071] rcu: blocking rcu_node structures (internal RCU debug):
[ 27.871331] Task dump for CPU 0:
[ 27.874555] task:systemd-udevd state:R running task stack:0 pid:227 ppid:198 flags:0x00000a0e
[ 27.884468] Call trace:
[ 27.886912] __switch_to+0xd4/0x130
[ 27.890401] 0xffff000801788000
Log 3:
Arago Project am62axx-evm -
Arago 2023.10 am62axx-evm -
am62axx-evm login: ***************************************************************
***************************************************************
NOTICE: This file system contains the following GPL-3.0 packages:
[ 20.617041] omap_i2c 20010000.i2c: controller timed out
Thanks for your help.
Maurice