Hi,
I have a new LogicPd Zoom board that fails to boot the OS demos from the SD cards.
I configured it according to the quick start guide at put the SD cards as instructed but it does not boot.
When I connect a UART (115200,n,8,1), I get this:
04 01 05 01 34 30 07 58 13 02 01 00 12 15 01 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00 00 14 15 01 00 00 00 00 00 00 00 00 00 00
00 00 00 00 00 00 00 00 00 00
(bytes are shown in hex since the data is not ASCII).
Any idea what is wrong?
Other info:
- The board is new, and I've never seen it work before.
- I tried SD cards in both MMC ports.
- I tried the Linux, SD and android SD cards.
Thanks,
Shay