This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDX654IDKEVM: Does No Boot Mode require ROM?

Part Number: TMDX654IDKEVM
Other Parts Discussed in Thread: CCSTUDIO

Hi,

I am trying to understand how No Boot mode works when connecting to CCStudio using a JTAG connection. When the SoC is in the No Boot configuration, and is powered on, is there ROM code that is executing to allow a JTAG interface?

Thanks.

  • JTAG interface operation is independent of ROM, so you can connect JTAG in no boot config on a general purpose device.  No Boot configuration will essentially fall into a NOP loop and not attempt to boot from any boot source.  

    Regards,

    James