Other Parts Discussed in Thread: TMS320C6746, OMAP-L138, OMAPL138
Hi,
I need to use USB on TMS320C6746 as a CDC class to communicate with the PC on virtual COM. I downloaded biosusb_01_10_03 which only supports HID and MSD.
Can anyone please clarify the following queries ?
1. What VID/PID has to be used for 6746?
2. From where can I get the inf file to support virtual COM?
3. To my knowledge, there is no CDC code support available from TI. In that case, is there any documentation which can be used to modify/write the class driver for CDC?
Thanks,
Mona Gandhi.