Other Parts Discussed in Thread: OMAP-L137
I am using C6747 on Spectrum Digital's OMAP-L137 evm board. I want to use a single I2S clock signal (bit clock and frame sync clock) to control both McASP0 and McASP1 for up to 28 channels, and to serve them using EDMA. However the AIC3106 codec is only connected to mcasp1. So i connect to the expansion board to use McASP0. How can i get the synchronized McASP0 and McASP1?