This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: System startup failure at remoteproc

Part Number: TDA4VM


Hi,TI

     Now we are small batch test on our custom TDA4VM. The occurrence of startup failure is accidental, the log as follows:

U-Boot 2021.01 (Dec 18 2023 - 11:53:42 +0800)

SoC:   J721E SR1.1 GP
Model: Texas Instruments K3 J721E SoC
EEPROM not available at 0x50, trying to read at 0x51
Reading on-board EEPROM at 0x51 failed -1
Board: J721EX-PM1-SOM rev E2
DRAM:  4 GiB
Flash: 0 Bytes
MMC:   sdhci@4f80000: 0, sdhci@4fb0000: 1
Loading Environment from FAT... OK
In:    serial@2800000
Out:   serial@2800000
Err:   serial@2800000
am65_cpsw_nuss ethernet@46000000: K3 CPSW: nuss_ver: 0x6BA00101 cpsw_ver: 0x6BA80100 ale_ver: 0x00293904 Ports:1 mdio_freq:1000000
EEPROM not available at 0x50, trying to read at 0x51
Reading on-board EEPROM at 0x51 failed -1
cdns,sierra serdes@5000000: sierra probed
Net:   eth0: ethernet@46000000port@1
ota_init
bootfirst=0, trycount=255, bootpart=1:2
 normal boot
switch to success partion: Saving Environment to FAT... OK
Hit any key to stop autoboot:  0 
switch to partitions #0, OK
mmc1 is current device
SD/MMC found on device 1
Failed to load 'boot.scr'
574 bytes read in 7 ms (80.1 KiB/s)
Loaded env from uEnv.txt
Importing environment from mmc1 ...
19079680 bytes read in 796 ms (22.9 MiB/s)
107839 bytes read in 12 ms (8.6 MiB/s)
## Flattened Device Tree blob at 88000000
   Booting using the fdt blob at 0x88000000
   Loading Device Tree to 000000008fee2000, end 000000008fffffff ... OK

Starting kernel ...

[    0.000000] Booting Linux on physical CPU 0x0000000000 [0x411fd080]
[    0.000000] Linux version 5.10.162-g76b3e88d56 (oe-user@oe-host) (aarch64-none-linux-gnu-gcc (GNU Toolchain for the A-profile Architecture 9.2-2019.12 (arm-9.10)) 9.2.1 20191025, GNU ld (GNU Toolchain for the A-profile Architecture 9.2-2019.12 (arm-9.10)) 2.33.1.20191209) #1 SMP PREEMPT Fri Mar 3 23:00:40 UTC 2023
[    0.000000] Machine model: Texas Instruments K3 J721E SoC
[    0.000000] earlycon: ns16550a0 at MMIO32 0x0000000002800000 (options '')
[    0.000000] printk: bootconsole [ns16550a0] enabled
[    0.000000] efi: UEFI not found.
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a0000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node r5f-dma-memory@a0000000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a0100000, size 15 MiB
[    0.000000] OF: reserved mem: initialized node r5f-memory@a0100000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a1000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node r5f-dma-memory@a1000000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a1100000, size 15 MiB
[    0.000000] OF: reserved mem: initialized node r5f-memory@a1100000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a2000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node r5f-dma-memory@a2000000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a2100000, size 15 MiB
[    0.000000] OF: reserved mem: initialized node r5f-memory@a2100000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a3000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node r5f-dma-memory@a3000000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a3100000, size 15 MiB
[    0.000000] OF: reserved mem: initialized node r5f-memory@a3100000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a4000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node r5f-dma-memory@a4000000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a4100000, size 15 MiB
[    0.000000] OF: reserved mem: initialized node r5f-memory@a4100000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a5000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node r5f-dma-memory@a5000000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a5100000, size 15 MiB
[    0.000000] OF: reserved mem: initialized node r5f-memory@a5100000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a6000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node c66-dma-memory@a6000000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a6100000, size 15 MiB
[    0.000000] OF: reserved mem: initialized node c66-memory@a6100000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a7000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node c66-dma-memory@a7000000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a7100000, size 15 MiB
[    0.000000] OF: reserved mem: initialized node c66-memory@a7100000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a8000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node c71-dma-memory@a8000000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a8100000, size 15 MiB
[    0.000000] OF: reserved mem: initialized node c71-memory@a8100000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000ac000000, size 2 MiB
[    0.000000] OF: reserved mem: initialized node r5f-virtual-eth-queues@ac000000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000ac200000, size 30 MiB
[    0.000000] OF: reserved mem: initialized node r5f-virtual-eth-buffers@ac200000, compatible id shared-dma-pool
[    0.000000] Zone ranges:
[    0.000000]   DMA      [mem 0x0000000080000000-0x00000000ffffffff]
[    0.000000]   DMA32    empty
[    0.000000]   Normal   [mem 0x0000000100000000-0x00000008ffffffff]
[    0.000000] Movable zone start for each node
[    0.000000] Early memory node ranges
[    0.000000]   node   0: [mem 0x0000000080000000-0x000000009e7fffff]
[    0.000000]   node   0: [mem 0x000000009e800000-0x00000000a8ffffff]
[    0.000000]   node   0: [mem 0x00000000a9000000-0x00000000a9ffffff]
[    0.000000]   node   0: [mem 0x00000000aa000000-0x00000000abbfffff]
[    0.000000]   node   0: [mem 0x00000000abc00000-0x00000000abffffff]
[    0.000000]   node   0: [mem 0x00000000ac000000-0x00000000adffffff]
[    0.000000]   node   0: [mem 0x00000000ae000000-0x00000000ffffffff]
[    0.000000]   node   0: [mem 0x0000000880000000-0x00000008ffffffff]
[    0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000008ffffffff]
[    0.000000] cma: Reserved 512 MiB at 0x00000000e0000000
[    0.000000] psci: probing for conduit method from DT.
[    0.000000] psci: PSCIv1.1 detected in firmware.
[    0.000000] psci: Using standard PSCI v0.2 function IDs
[    0.000000] psci: Trusted OS migration not required
[    0.000000] psci: SMC Calling Convention v1.2
[    0.000000] percpu: Embedded 22 pages/cpu s50392 r8192 d31528 u90112
[    0.000000] Detected PIPT I-cache on CPU0
[    0.000000] CPU features: detected: GIC system register CPU interface
[    0.000000] CPU features: detected: EL2 vector hardening
[    0.000000] CPU features: detected: ARM errata 1165522, 1319367, or 1530923
[    0.000000] CPU features: detected: Spectre-BHB
[    0.000000] CPU features: detected: ARM erratum 1742098
[    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 1032192
[    0.000000] Kernel command line: console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000 mtdparts=47040000.spi.0:512k(ospi.tiboot3),2m(ospi.tispl),4m(ospi.u-boot),256k(ospi.env),1m(ospi.sysfw),256k(ospi.env.backup),57088k@8m(ospi.rootfs),256k(ospi.phypattern);47034000.hyperbus:512k(hbmc.tiboot3),2m(hbmc.tispl),4m(hbmc.u-boot),256k(hbmc.env),1m(hbmc.sysfw),-@8m(hbmc.rootfs) root=PARTUUID=f42c8474-02 rw rootfstype=ext4 rootwait
[    0.000000] Dentry cache hash table entries: 524288 (order: 10, 4194304 bytes, linear)
[    0.000000] Inode-cache hash table entries: 262144 (order: 9, 2097152 bytes, linear)
[    0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
[    0.000000] software IO TLB: mapped [mem 0x00000000dc000000-0x00000000e0000000] (64MB)
[    0.000000] Memory: 3271324K/4194304K available (11200K kernel code, 1160K rwdata, 4300K rodata, 1856K init, 433K bss, 398692K reserved, 524288K cma-reserved)
[    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
[    0.000000] rcu: Preemptible hierarchical RCU implementation.
[    0.000000] rcu: 	RCU event tracing is enabled.
[    0.000000] rcu: 	RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=2.
[    0.000000] 	Trampoline variant of Tasks RCU enabled.
[    0.000000] 	Tracing variant of Tasks RCU enabled.
[    0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[    0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2
[    0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[    0.000000] GICv3: GIC: Using split EOI/Deactivate mode
[    0.000000] GICv3: 960 SPIs implemented
[    0.000000] GICv3: 0 Extended SPIs implemented
[    0.000000] GICv3: Distributor has no Range Selector support
[    0.000000] GICv3: 16 PPIs implemented
[    0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000001900000
[    0.000000] ITS [mem 0x01820000-0x0182ffff]
[    0.000000] GIC: enabling workaround for ITS: Socionext Synquacer pre-ITS
[    0.000000] ITS@0x0000000001820000: Devices Table too large, reduce ids 20->19
[    0.000000] ITS@0x0000000001820000: allocated 524288 Devices @880800000 (flat, esz 8, psz 64K, shr 0)
[    0.000000] ITS: using cache flushing for cmd queue
[    0.000000] GICv3: using LPI property table @0x0000000880030000
[    0.000000] GIC: using cache flushing for LPI property table
[    0.000000] GICv3: CPU0: using allocated LPI pending table @0x0000000880040000
[    0.000000] arch_timer: cp15 timer(s) running at 200.00MHz (phys).
[    0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x2e2049d3e8, max_idle_ns: 440795210634 ns
[    0.000002] sched_clock: 56 bits at 200MHz, resolution 5ns, wraps every 4398046511102ns
[    0.008430] Console: colour dummy device 80x25
[    0.012991] Calibrating delay loop (skipped), value calculated using timer frequency.. 400.00 BogoMIPS (lpj=800000)
[    0.023661] pid_max: default: 32768 minimum: 301
[    0.028416] LSM: Security Framework initializing
[    0.033169] Mount-cache hash table entries: 8192 (order: 4, 65536 bytes, linear)
[    0.040746] Mountpoint-cache hash table entries: 8192 (order: 4, 65536 bytes, linear)
[    0.049564] rcu: Hierarchical SRCU implementation.
[    0.054631] Platform MSI: msi-controller@1820000 domain created
[    0.060860] PCI/MSI: /bus@100000/interrupt-controller@1800000/msi-controller@1820000 domain created
[    0.070164] EFI services will not be available.
[    0.074883] smp: Bringing up secondary CPUs ...
I/TC: Secondary CPU 1 initializing
I/TC: Secondary CPU 1 switching to normal world boot
[    0.088135] Detected PIPT I-cache on CPU1
[    0.088159] GICv3: CPU1: found redistributor 1 region 0:0x0000000001920000
[    0.088170] GICv3: CPU1: using allocated LPI pending table @0x0000000880050000
[    0.088204] CPU1: Booted secondary processor 0x0000000001 [0x411fd080]
[    0.088253] smp: Brought up 1 node, 2 CPUs
[    0.117598] SMP: Total of 2 processors activated.
[    0.122404] CPU features: detected: 32-bit EL0 Support
[    0.127658] CPU features: detected: CRC32 instructions
[    0.141614] CPU: All CPU(s) started at EL2
[    0.145809] alternatives: patching kernel code
[    0.150817] devtmpfs: initialized
[    0.159491] KASLR disabled due to lack of seed
[    0.164132] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[    0.174096] futex hash table entries: 512 (order: 3, 32768 bytes, linear)
[    0.186937] pinctrl core: initialized pinctrl subsystem
[    0.192584] DMI not present or invalid.
[    0.196827] NET: Registered protocol family 16
[    0.202021] DMA: preallocated 512 KiB GFP_KERNEL pool for atomic allocations
[    0.209324] DMA: preallocated 512 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
[    0.217371] DMA: preallocated 512 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
[    0.225668] thermal_sys: Registered thermal governor 'step_wise'
[    0.225671] thermal_sys: Registered thermal governor 'power_allocator'
[    0.232239] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[    0.245873] ASID allocator initialised with 65536 entries
[    0.268202] HugeTLB registered 1.00 GiB page size, pre-allocated 0 pages
[    0.275058] HugeTLB registered 32.0 MiB page size, pre-allocated 0 pages
[    0.281907] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages
[    0.288754] HugeTLB registered 64.0 KiB page size, pre-allocated 0 pages
[    0.296213] cryptd: max_cpu_qlen set to 1000
[    0.302232] k3-chipinfo 43000014.chipid: Family:J721E rev:SR2.0 JTAGID[0x1bb6402f] Detected
[    0.311038] vsys_3v3: supplied by evm_12v0
[    0.315391] vsys_5v0: supplied by evm_12v0
[    0.319699] vdd_mmc1: supplied by vsys_3v3
[    0.324488] iommu: Default domain type: Translated 
[    0.329615] SCSI subsystem initialized
[    0.333635] mc: Linux media interface: v0.10
[    0.338003] videodev: Linux video capture interface: v2.00
[    0.343633] pps_core: LinuxPPS API ver. 1 registered
[    0.348703] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[    0.358043] PTP clock support registered
[    0.362061] EDAC MC: Ver: 3.0.0
[    0.365848] FPGA manager framework
[    0.369355] Advanced Linux Sound Architecture Driver Initialized.
[    0.375949] clocksource: Switched to clocksource arch_sys_counter
[    0.382275] VFS: Disk quotas dquot_6.6.0
[    0.386305] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[    0.395859] NET: Registered protocol family 2
[    0.400596] IP idents hash table entries: 65536 (order: 7, 524288 bytes, linear)
[    0.409171] tcp_listen_portaddr_hash hash table entries: 2048 (order: 3, 32768 bytes, linear)
[    0.417929] TCP established hash table entries: 32768 (order: 6, 262144 bytes, linear)
[    0.426127] TCP bind hash table entries: 32768 (order: 7, 524288 bytes, linear)
[    0.433923] TCP: Hash tables configured (established 32768 bind 32768)
[    0.440720] UDP hash table entries: 2048 (order: 4, 65536 bytes, linear)
[    0.447615] UDP-Lite hash table entries: 2048 (order: 4, 65536 bytes, linear)
[    0.455011] NET: Registered protocol family 1
[    0.459724] RPC: Registered named UNIX socket transport module.
[    0.465788] RPC: Registered udp transport module.
[    0.470592] RPC: Registered tcp transport module.
[    0.475395] RPC: Registered tcp NFSv4.1 backchannel transport module.
[    0.481977] NET: Registered protocol family 44
[    0.486522] PCI: CLS 0 bytes, default 64
[    0.490861] hw perfevents: enabled with armv8_cortex_a72 PMU driver, 7 counters available
[    0.501208] Initialise system trusted keyrings
[    0.505822] workingset: timestamp_bits=46 max_order=20 bucket_order=0
[    0.513954] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[    0.520230] NFS: Registering the id_resolver key type
[    0.525420] Key type id_resolver registered
[    0.529693] Key type id_legacy registered
[    0.533812] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[    0.540660] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...
[    0.548303] 9p: Installing v9fs 9p2000 file system support
[    0.573991] Key type asymmetric registered
[    0.578178] Asymmetric key parser 'x509' registered
[    0.583174] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 243)
[    0.590733] io scheduler mq-deadline registered
[    0.595358] io scheduler kyber registered
[    0.601014] pinctrl-single 4301c000.pinctrl: 94 pins, size 376
[    0.607181] pinctrl-single 11c000.pinctrl: 173 pins, size 692
[    0.615922] ti-pat 31010000.pat: Found PAT Rev 1.0 with 16384 pages
[    0.622361] debugfs: Directory '31010000.pat' with parent 'regmap' already present!
[    0.630348] ti-pat 31011000.pat: Found PAT Rev 1.0 with 16384 pages
[    0.636768] debugfs: Directory '31011000.pat' with parent 'regmap' already present!
[    0.644716] ti-pat 31012000.pat: Found PAT Rev 1.0 with 16384 pages
[    0.651134] debugfs: Directory '31012000.pat' with parent 'regmap' already present!
[    0.659061] ti-pat 31013000.pat: Found PAT Rev 1.0 with 2048 pages
[    0.665386] debugfs: Directory '31013000.pat' with parent 'regmap' already present!
[    0.673328] ti-pat 31014000.pat: Found PAT Rev 1.0 with 2048 pages
[    0.679653] debugfs: Directory '31014000.pat' with parent 'regmap' already present!
[    0.689297] Serial: 8250/16550 driver, 10 ports, IRQ sharing enabled
[    0.697450] arm-smmu-v3 36600000.iommu: ias 48-bit, oas 48-bit (features 0x00001faf)
[    0.705664] arm-smmu-v3 36600000.iommu: allocated 65536 entries for cmdq
[    0.712698] arm-smmu-v3 36600000.iommu: allocated 32768 entries for evtq
[    0.721156] arm-smmu-v3 36600000.iommu: msi_domain absent - falling back to wired irqs
[    0.734243] brd: module loaded
[    0.740674] loop: module loaded
[    0.744368] megasas: 07.714.04.00-rc1
[    0.749950] tun: Universal TUN/TAP device driver, 1.6
[    0.755397] igbvf: Intel(R) Gigabit Virtual Function Network Driver
[    0.761807] igbvf: Copyright (c) 2009 - 2012 Intel Corporation.
[    0.767879] sky2: driver version 1.30
[    0.772128] VFIO - User Level meta-driver version: 0.3
[    0.777868] i2c /dev entries driver
[    0.782274] sdhci: Secure Digital Host Controller Interface driver
[    0.788612] sdhci: Copyright(c) Pierre Ossman
[    0.793258] sdhci-pltfm: SDHCI platform and OF driver helper
[    0.799618] ledtrig-cpu: registered to indicate activity on CPUs
[    0.805934] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....
[    0.813262] optee: probing for conduit method.
I/TC: Reserved shared memory is enabled
I/TC: Dynamic shared memory is enabled
I/TC: Normal World virtualization support is disabled
I/TC: Asynchronous notifications are disabled
[    0.817823] optee: revision 3.20 (8e74d476)
[    0.834223] optee: dynamic shared memory is enabled
[    0.843691] optee: initialized driver
[    0.848758] NET: Registered protocol family 17
[    0.853386] 9pnet: Installing 9P2000 support
[    0.857789] Key type dns_resolver registered
[    0.862236] Loading compiled-in X.509 certificates
[    0.874175] ti-sci 44083000.dmsc: ABI: 3.1 (firmware rev 0x0008 '8.6.3--v08.06.03 (Chill Capybar')
[    0.947133] davinci-mcasp 2ba0000.mcasp: IRQ common not found
[    0.954991] omap_i2c 2000000.i2c: bus 0 rev0.12 at 400 kHz
[    0.961064] omap_i2c 2010000.i2c: bus 1 rev0.12 at 100 kHz
[    0.967421] pca953x 2-0022: supply vcc not found, using dummy regulator
[    0.974242] pca953x 2-0022: using AI
[    1.000576] gpio-496 (PRG1_RGMII_INT): hogged as output/high
[    1.006554] gpio-497 (PRG0_RGMII_INT): hogged as output/high
[    1.012530] gpio-499 (ENET_RGMII_PWRDN_EN): hogged as output/high
[    1.018948] gpio-500 (VSYS_1V0_CSI_EN): hogged as output/high
[    1.025012] gpio-501 (HDMI_PWRDN_EN): hogged as output/high
[    1.030897] gpio-502 (CSI_PWRDN_EN1): hogged as output/high
[    1.036785] gpio-503 (CSI_PWRDN_EN2): hogged as output/high
[    1.042935] gpio-506 (VSYS_3V3_PCIE2_EN): hogged as output/high
[    1.049179] gpio-507 (EXP_3V3_WIFI_EN): hogged as output/high
[    1.055242] gpio-508 (MAX96712_STB): hogged as output/high
[    1.061040] gpio-509 (MAX96712_STB1): hogged as output/high
[    1.066925] gpio-510 (LT9611_RST): hogged as output/high
[    1.072545] gpio-511 (GPS_PWR_EN): hogged as output/high
[    1.078208] omap_i2c 2060000.i2c: bus 2 rev0.12 at 400 kHz
[    1.084715] ti-sci-intr bus@100000:bus@28380000:interrupt-controller2: Interrupt Router 137 domain created
[    1.094701] ti-sci-intr bus@100000:interrupt-controller0: Interrupt Router 131 domain created
[    1.103521] ti-sci-intr bus@100000:main-navss:interrupt-controller1: Interrupt Router 213 domain created
[    1.113408] ti-sci-inta 33d00000.interrupt-controller: Interrupt Aggregator domain 209 created
[    1.135945] j721e-pcie 2900000.pcie: host bridge /bus@100000/pcie@2900000 ranges:
[    1.143642] j721e-pcie 2900000.pcie:       IO 0x0010001000..0x0010010fff -> 0x0010001000
[    1.151920] j721e-pcie 2900000.pcie:      MEM 0x0010011000..0x0017ffffff -> 0x0010011000
[    1.160201] j721e-pcie 2900000.pcie:   IB MEM 0x0000000000..0xffffffffffff -> 0x0000000000
[    2.176403] j721e-pcie 2900000.pcie: PCI host bridge to bus 0000:00
[    2.182817] pci_bus 0000:00: root bus resource [bus 00-ff]
[    2.188423] pci_bus 0000:00: root bus resource [io  0x0000-0xffff] (bus address [0x10001000-0x10010fff])
[    2.198113] pci_bus 0000:00: root bus resource [mem 0x10011000-0x17ffffff]
[    2.205166] pci 0000:00:00.0: [104c:b00d] type 01 class 0x060400
[    2.211305] pci_bus 0000:00: 2-byte config write to 0000:00:00.0 offset 0x4 may corrupt adjacent RW1C bits
[    2.221254] pci 0000:00:00.0: supports D1
[    2.225348] pci 0000:00:00.0: PME# supported from D0 D1 D3hot
[    2.231234] pci 0000:00:00.0: reg 0x224: [mem 0x00000000-0x003fffff 64bit]
[    2.238261] pci 0000:00:00.0: VF(n) BAR0 space: [mem 0x00000000-0x00ffffff 64bit] (contains BAR0 for 4 VFs)
[    2.250357] pci 0000:00:00.0: bridge configuration invalid ([bus 00-00]), reconfiguring
[    2.260425] pci_bus 0000:01: busn_res: [bus 01-ff] end is updated to 01
[    2.267196] pci 0000:00:00.0: BAR 7: assigned [mem 0x10400000-0x113fffff 64bit]
[    2.274669] pci 0000:00:00.0: PCI bridge to [bus 01]
[    2.279972] pcieport 0000:00:00.0: PME: Signaling with IRQ 61
[    2.286345] j721e-pcie 2910000.pcie: host bridge /bus@100000/pcie@2910000 ranges:
[    2.294016] j721e-pcie 2910000.pcie:       IO 0x0018001000..0x0018010fff -> 0x0018001000
[    2.302293] j721e-pcie 2910000.pcie:      MEM 0x0018011000..0x001fffffff -> 0x0018011000
[    2.310573] j721e-pcie 2910000.pcie:   IB MEM 0x0000000000..0xffffffffffff -> 0x0000000000
[    2.395589] j721e-pcie 2910000.pcie: LINK DOWN!
[    3.323778] j721e-pcie 2910000.pcie: PCI host bridge to bus 0001:00
[    3.330191] pci_bus 0001:00: root bus resource [bus 00-ff]
[    3.335797] pci_bus 0001:00: root bus resource [io  0x10000-0x1ffff] (bus address [0x18001000-0x18010fff])
[    3.345665] pci_bus 0001:00: root bus resource [mem 0x18011000-0x1fffffff]
[    3.352715] pci 0001:00:00.0: [104c:b00d] type 01 class 0x060400
[    3.358854] pci_bus 0001:00: 2-byte config write to 0001:00:00.0 offset 0x4 may corrupt adjacent RW1C bits
[    3.368784] pci 0001:00:00.0: supports D1
[    3.372878] pci 0001:00:00.0: PME# supported from D0 D1 D3hot
[    3.380854] pci 0001:00:00.0: bridge configuration invalid ([bus 00-00]), reconfiguring
[    3.390953] pci_bus 0001:01: busn_res: [bus 01-ff] end is updated to 01
[    3.397720] pci 0001:00:00.0: PCI bridge to [bus 01]
[    3.402991] pcieport 0001:00:00.0: PME: Signaling with IRQ 64
[    3.409857] k3-ringacc 2b800000.ringacc: Ring Accelerator probed rings:286, gp-rings[96,20] sci-dev-id:235
[    3.419743] k3-ringacc 2b800000.ringacc: dma-ring-reset-quirk: disabled
[    3.426503] k3-ringacc 2b800000.ringacc: RA Proxy rev. 66346100, num_proxies:64
[    3.435469] k3-ringacc 3c000000.ringacc: Ring Accelerator probed rings:1024, gp-rings[440,150] sci-dev-id:211
[    3.445618] k3-ringacc 3c000000.ringacc: dma-ring-reset-quirk: disabled
[    3.452384] k3-ringacc 3c000000.ringacc: RA Proxy rev. 66346100, num_proxies:64
[    3.460342] printk: console [ttyS2] disabled
[    3.464735] 2800000.serial: ttyS2 at MMIO 0x2800000 (irq = 20, base_baud = 3000000) is a 8250
[    3.473479] printk: console [ttyS2] enabled
[    3.473479] printk: console [ttyS2] enabled
[    3.481915] printk: bootconsole [ns16550a0] disabled
[    3.481915] printk: bootconsole [ns16550a0] disabled
[    3.492425] 2810000.serial: ttyS3 at MMIO 0x2810000 (irq = 21, base_baud = 3000000) is a 8250
[    3.501399] 2840000.serial: ttyS6 at MMIO 0x2840000 (irq = 22, base_baud = 3000000) is a 8250
[    3.512170] cdns-ufshcd 4e84000.ufs: ufshcd_populate_vreg: Unable to find vdd-hba-supply regulator, assuming enabled
[    3.522680] cdns-ufshcd 4e84000.ufs: ufshcd_populate_vreg: Unable to find vcc-supply regulator, assuming enabled
[    3.532834] cdns-ufshcd 4e84000.ufs: ufshcd_populate_vreg: Unable to find vccq-supply regulator, assuming enabled
[    3.543076] cdns-ufshcd 4e84000.ufs: ufshcd_populate_vreg: Unable to find vccq2-supply regulator, assuming enabled
[    3.554332] scsi host0: ufshcd
[    3.562143] am65-cpts 310d0000.cpts: CPTS ver 0x4e8a010a, freq:200000000, add_val:4 pps:0
[    3.671896] davinci-mcasp 2ba0000.mcasp: IRQ common not found
[    3.677792] mmc0: CQHCI version 5.10
[    3.688654] omap-mailbox 31f80000.mailbox: omap mailbox rev 0x66fc7100
[    3.695537] omap-mailbox 31f81000.mailbox: omap mailbox rev 0x66fc7100
[    3.702390] omap-mailbox 31f82000.mailbox: omap mailbox rev 0x66fc7100
[    3.709239] omap-mailbox 31f83000.mailbox: omap mailbox rev 0x66fc7100
[    3.716069] omap-mailbox 31f84000.mailbox: omap mailbox rev 0x66fc7100
[    3.718550] mmc0: SDHCI controller on 4f80000.mmc [4f80000.mmc] using ADMA 64-bit
[    3.726883] ti-udma 285c0000.dma-controller: Channels: 26 (tchan: 13, rchan: 13, gp-rflow: 8)
[    3.740861] ti-udma 31150000.dma-controller: Channels: 122 (tchan: 61, rchan: 61, gp-rflow: 16)
[    3.753238] davinci-mcasp 2ba0000.mcasp: IRQ common not found
[    3.768910] mmc1: CQHCI version 5.10
[    3.772934] debugfs: Directory 'pd:27' with parent 'pm_genpd' already present!
[    3.780259] debugfs: Directory 'pd:26' with parent 'pm_genpd' already present!
[    3.788646] debugfs: Directory 'pd:242' with parent 'pm_genpd' already present!
[    3.795977] debugfs: Directory 'pd:241' with parent 'pm_genpd' already present!
[    3.803298] debugfs: Directory 'pd:240' with parent 'pm_genpd' already present!
[    3.810608] debugfs: Directory 'pd:239' with parent 'pm_genpd' already present!
[    3.840410] ALSA device list:
[    3.843383]   No soundcards found.
[    3.848115] mmc0: Command Queue Engine enabled
[    3.852556] mmc0: new HS200 MMC card at address 0001
[    3.857811] mmcblk0: mmc0:0001 S0J57X 29.6 GiB 
[    3.862452] mmcblk0boot0: mmc0:0001 S0J57X partition 1 31.5 MiB
[    3.868471] mmcblk0boot1: mmc0:0001 S0J57X partition 2 31.5 MiB
[    3.874460] mmcblk0rpmb: mmc0:0001 S0J57X partition 3 4.00 MiB, chardev (237:0)
[    3.965375] cdns-ufshcd 4e84000.ufs: link startup failed 1
[    3.970861] cdns-ufshcd 4e84000.ufs: UFS Host state=0
[    3.975899] cdns-ufshcd 4e84000.ufs: outstanding reqs=0x0 tasks=0x0
[    3.982151] cdns-ufshcd 4e84000.ufs: saved_err=0x0, saved_uic_err=0x0
[    3.988576] cdns-ufshcd 4e84000.ufs: Device power mode=1, UIC link state=0
[    3.995433] cdns-ufshcd 4e84000.ufs: PM in progress=0, sys. suspended=0
[    4.002031] cdns-ufshcd 4e84000.ufs: Auto BKOPS=0, Host self-block=0
[    4.008369] cdns-ufshcd 4e84000.ufs: Clk gate=1
[    4.012887] cdns-ufshcd 4e84000.ufs: last_hibern8_exit_tstamp at 0 us, hibern8_exit_cnt=0
[    4.021045] cdns-ufshcd 4e84000.ufs: last intr at 3876307 us, last intr status=0x404
[    4.028771] cdns-ufshcd 4e84000.ufs: error handling flags=0x0, req. abort count=0
[    4.036236] cdns-ufshcd 4e84000.ufs: hba->ufs_version=0x210, Host capabilities=0x1587031f, caps=0x0
[    4.045260] cdns-ufshcd 4e84000.ufs: quirks=0x0, dev. quirks=0x0
[    4.051252] cdns-ufshcd 4e84000.ufs: clk: core_clk, rate: 250000000
[    4.057503] cdns-ufshcd 4e84000.ufs: clk: phy_clk, rate: 19200000
[    4.063582] cdns-ufshcd 4e84000.ufs: clk: ref_clk, rate: 19200000
[    4.069661] cdns-ufshcd 4e84000.ufs: ufshcd_print_pwr_info:[RX, TX]: gear=[0, 0], lane[0, 0], pwr[INVALID MODE, INVALID MODE], rate = 0
[    4.081821] host_regs: 00000000: 1587031f 00000000 00000210 00000000
[    4.088169] host_regs: 00000010: 00000000 00000000 00000000 00000000
[    4.094508] host_regs: 00000020: 00000000 00000470 00000000 00000000
[    4.100846] host_regs: 00000030: 00000008 00000001 00000000 00000000
[    4.107183] host_regs: 00000040: 00000000 00000000 00000000 00000000
[    4.113521] host_regs: 00000050: 00000000 00000000 00000000 00000000
[    4.119858] host_regs: 00000060: 00000000 00000000 00000000 00000000
[    4.126195] host_regs: 00000070: 00000000 00000000 00000000 00000000
[    4.132532] host_regs: 00000080: 00000000 00000000 00000000 00000000
[    4.138870] host_regs: 00000090: 00000000 00000000 00000000 00000000
[    4.145208] cdns-ufshcd 4e84000.ufs: No record of pa_err
[    4.150508] cdns-ufshcd 4e84000.ufs: No record of dl_err
[    4.155805] cdns-ufshcd 4e84000.ufs: No record of nl_err
[    4.161102] cdns-ufshcd 4e84000.ufs: No record of tl_err
[    4.166399] cdns-ufshcd 4e84000.ufs: No record of dme_err
[    4.171783] cdns-ufshcd 4e84000.ufs: No record of auto_hibern8_err
[    4.177947] cdns-ufshcd 4e84000.ufs: No record of fatal_err
[    4.183504] cdns-ufshcd 4e84000.ufs: link_startup_fail[0] = 0x1 at 3877426 us
[    4.190625] cdns-ufshcd 4e84000.ufs: No record of resume_fail
[    4.196356] cdns-ufshcd 4e84000.ufs: No record of suspend_fail
[    4.202173] cdns-ufshcd 4e84000.ufs: No record of dev_reset
[    4.207731] cdns-ufshcd 4e84000.ufs: No record of host_reset
[    4.213377] cdns-ufshcd 4e84000.ufs: No record of task_abort
[    4.836325] mmc1: SDHCI controller on 4fb0000.mmc [4fb0000.mmc] using ADMA 64-bit
[    4.844631] Waiting for root device PARTUUID=f42c8474-02...
[    4.902456] mmc1: new ultra high speed DDR50 SDHC card at address aaaa
[    4.909301] mmcblk1: mmc1:aaaa SD32G 29.7 GiB 
[    4.914956]  mmcblk1: p1 p2
[    4.984580] EXT4-fs (mmcblk1p2): recovery complete
[    4.990160] EXT4-fs (mmcblk1p2): mounted filesystem with ordered data mode. Opts: (null)
[    4.998267] VFS: Mounted root (ext4 filesystem) on device 179:98.
[    5.008786] devtmpfs: mounted
[    5.012568] Freeing unused kernel memory: 1856K
[    5.017195] Run /sbin/init as init process
[    5.200546] systemd[1]: System time before build time, advancing clock.
[    5.261162] NET: Registered protocol family 10
[    5.266037] Segment Routing with IPv6
[    5.298463] systemd[1]: systemd 244.5+ running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR -SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN2 -IDN -PCRE2 default-hierarchy=hybrid)
[    5.320227] systemd[1]: Detected architecture arm64.

Welcome to Arago 2021.09!

[    5.360486] systemd[1]: Set hostname to <j7-evm>.
[    5.544795] systemd[1]: /lib/systemd/system/irqbalanced.service:6: Unknown key name 'ConditionCPUs' in section 'Unit', ignoring.
[    5.569094] systemd[1]: /lib/systemd/system/docker.socket:6: ListenStream= references a path below legacy directory /var/run/, updating /var/run/docker.sock → /run/docker.sock; please update the unit file accordingly.
[    5.640882] random: systemd: uninitialized urandom read (16 bytes read)
[    5.649187] systemd[1]: Created slice system-getty.slice.
[  OK  ] Created slice system-getty.slice.
[    5.672028] random: systemd: uninitialized urandom read (16 bytes read)
[    5.679380] systemd[1]: Created slice system-serial\x2dgetty.slice.
[  OK  ] Created slice system-serial\x2dgetty.slice.
[    5.700027] random: systemd: uninitialized urandom read (16 bytes read)
[    5.707260] systemd[1]: Created slice User and Session Slice.
[  OK  ] Created slice User and Session Slice.
[    5.728158] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
[  OK  ] Started Dispatch Password …ts to Console Directory Watch.
[    5.752081] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
[  OK  ] Started Forward Password R…uests to Wall Directory Watch.
[    5.776069] systemd[1]: Reached target Paths.
[  OK  ] Reached target Paths.
[    5.792018] systemd[1]: Reached target Remote File Systems.
[  OK  ] Reached target Remote File Systems.
[    5.812004] systemd[1]: Reached target Slices.
[  OK  ] Reached target Slices.
[    5.828011] systemd[1]: Reached target Swap.
[  OK  ] Reached target Swap.
[    5.861544] systemd[1]: Listening on RPCbind Server Activation Socket.
[  OK  ] Listening on RPCbind Server Activation Socket.
[    5.884085] systemd[1]: Reached target RPC Port Mapper.
[  OK  ] Reached target RPC Port Mapper.
[    5.906440] systemd[1]: Listening on Process Core Dump Socket.
[  OK  ] Listening on Process Core Dump Socket.
[    5.928179] systemd[1]: Listening on initctl Compatibility Named Pipe.
[  OK  ] Listening on initctl Compatibility Named Pipe.
[    5.953576] systemd[1]: Condition check resulted in Journal Audit Socket being skipped.
[    5.961917] systemd[1]: Listening on Journal Socket (/dev/log).
[  OK  ] Listening on Journal Socket (/dev/log).
[    5.984265] systemd[1]: Listening on Journal Socket.
[  OK  ] Listening on Journal Socket.
[    6.000324] systemd[1]: Listening on Network Service Netlink Socket.
[  OK  ] Listening on Network Service Netlink Socket.
[    6.024223] systemd[1]: Listening on udev Control Socket.
[  OK  ] Listening on udev Control Socket.
[    6.044155] systemd[1]: Listening on udev Kernel Socket.
[  OK  ] Listening on udev Kernel Socket.
[    6.066198] systemd[1]: Mounting Huge Pages File System...
         Mounting Huge Pages File System...
[    6.082165] systemd[1]: Mounting POSIX Message Queue File System...
         Mounting POSIX Message Queue File System...
[    6.106247] systemd[1]: Mounting Kernel Debug File System...
         Mounting Kernel Debug File System...
[    6.126716] systemd[1]: Mounting Temporary Directory (/tmp)...
         Mounting Temporary Directory (/tmp)...
[    6.146356] systemd[1]: Starting Create list of static device nodes for the current kernel...
         Starting Create list of st…odes for the current kernel...
[    6.176075] systemd[1]: Starting Start psplash boot splash screen...
         Starting Start psplash boot splash screen...
[    6.203149] systemd[1]: Starting RPC Bind...
         Starting RPC Bind...
[    6.216189] systemd[1]: Condition check resulted in File System Check on Root Device being skipped.
[    6.228446] systemd[1]: Starting Journal Service...
         Starting Journal Service...
[    6.252508] systemd[1]: Starting Load Kernel Modules...
         Starting Load Kernel Modules...
[    6.270445] systemd[1]: Starting Remount Root and Kernel File Systems...
[    6.277432] cryptodev: loading out-of-tree module taints kernel.
         Starting Remount Root and Kernel File Systems EXT4-fs (mmcblk1p2): re-mounted. Opts: (null)
[0m...
[    6.294788] cryptodev: driver 1.10 loaded.
[    6.306415] systemd[1]: Starting udev Coldplug all Devices...
         Starting udev Coldplug all Devices...
[    6.326777] systemd[1]: Started RPC Bind.
[  OK  ] Started RPC Bind.
[    6.340380] systemd[1]: Started Journal Service.
[  OK  ] Started Journal Service.
[  OK  ] Mounted Huge Pages File System.
[  OK  ] Mounted POSIX Message Queue File System.
[  OK  ] Mounted Kernel Debug File System.
[  OK  ] Mounted Temporary Directory (/tmp).
[  OK  ] Started Create list of sta… nodes for the current kernel.
[FAILED] Failed to start Start psplash boot splash screen.
See 'systemctl status psplash-start.service' for details.
[DEPEND] Dependency failed for Star…progress communication helper.
[  OK  ] Started Load Kernel Modules.
[  OK  ] Started Remount Root and Kernel File Systems.
         Mounting Kernel Configuration File System...
         Starting Flush Journal to Persistent Storage...
         Starting Apply Kernel Variables...
[    6.569422] systemd-journald[171]: Received client request to flush runtime journal.
         Starting Create Static Device Nodes in /dev...
[  OK  ] Mounted Kernel Configuration File System.
[  OK  ] Started Flush Journal to Persistent Storage.
[  OK  ] Started Apply Kernel Variables.
[  OK  ] Started Create Static Device Nodes in /dev.
[    6.664579] random: systemd: uninitialized urandom read (16 bytes read)
[  OK  ] Reached target Local File Systems (Pre).
[    6.688095] random: systemd: uninitialized urandom read (16 bytes read)
         Mounting /media/ram...
[    6.698485] random: systemd-journal: uninitialized urandom read (16 bytes read)
         Mounting /var/volatile...
         Starting udev Kernel Device Manager...
[  OK  ] Started udev Coldplug all Devices.
[  OK  ] Mounted /media/ram.
[  OK  ] Mounted /var/volatile.
         Starting udev Wait for Complete Device Initialization...
         Starting Load/Save Random Seed...
[  OK  ] Reached target Local File Systems.
         Starting Create Volatile Files and Directories...
[  OK  ] Started udev Kernel Device Manager.
[  OK  ] Started Create Volatile Files and Directories.
         Starting Network Time Synchronization...
         Starting Update UTMP about System Boot/Shutdown...
[  OK  ] Started Update UTMP about System Boot/Shutdown.
[  OK  ] Started Network Time Synchronization.
[  OK  ] Reached target System Time Set.
[  OK  ] Reached target System Time Synchronized.
[    7.102564] CAN device driver interface
[    7.102887] random: crng init done
[    7.109870] random: 66 urandom warning(s) missed due to ratelimiting
[  OK  ] Started Load/Save Random Seed.
[    7.135338] m_can_platform 2701000.can: m_can device registered (irq=38, version=32)
[    7.172602] m_can_platform 2721000.can: m_can device registered (irq=40, version=32)
[    7.181157] rtc-ds1307 0-006f: registered as rtc0
[    7.187096] rtc-ds1307 0-006f: setting system clock to 2024-01-11T16:05:44 UTC (1704989144)
[    7.219741] m_can_platform 2741000.can: m_can device registered (irq=42, version=32)
[    7.231065] k3-dsp-rproc 4d80800000.dsp: assigned reserved memory node c66-dma-memory@a7000000
[    7.244244] k3-dsp-rproc 4d80800000.dsp: configured DSP for remoteproc mode
[    7.245526] m_can_platform 2751000.can: m_can device registered (irq=44, version=32)
[    7.259012] k3-dsp-rproc 4d80800000.dsp: local reset is deasserted for device
[    7.266613] remoteproc remoteproc0: 4d80800000.dsp is available
[    7.277402] m_can_platform 2761000.can: m_can device registered (irq=46, version=32)
[    7.285710] k3-dsp-rproc 4d81800000.dsp: assigned reserved memory node c66-dma-memory@a6000000
[    7.301568] k3-dsp-rproc 4d81800000.dsp: configured DSP for remoteproc mode
[    7.310926] m_can_platform 2771000.can: m_can device registered (irq=48, version=32)
[    7.322329] k3-dsp-rproc 4d81800000.dsp: local reset is deasserted for device
[    7.332204] remoteproc remoteproc1: 4d81800000.dsp is available
[    7.338312] remoteproc remoteproc0: powering up 4d80800000.dsp
[    7.344304] remoteproc remoteproc0: Booting fw image j7-c66_0-fw, size 144652
[    7.356745] k3-dsp-rproc 64800000.dsp: assigned reserved memory node c71-dma-memory@a8000000
[    7.365869] pvrsrvkm 4e20000000.gpu: More than one power domain for this GPU, gpu driver manages power domains
[    7.376665] k3-dsp-rproc 4d80800000.dsp: booting DSP core using boot addr = 0xa6200400
[    7.386476] m_can_platform 2791000.can: m_can device registered (irq=50, version=32)
[    7.395768]  remoteproc0#vdev0buffer: assigned reserved memory node c66-dma-memory@a7000000
[    7.406651] virtio_rpmsg_bus virtio0: rpmsg host is online
[    7.414541] k3-dsp-rproc 64800000.dsp: configured DSP for remoteproc mode
[    7.421453]  remoteproc0#vdev0buffer: registered virtio0 (type 7)
[    7.427613] remoteproc remoteproc0: remote processor 4d80800000.dsp is now up
[    7.434899] remoteproc remoteproc1: powering up 4d81800000.dsp
[    7.440813] remoteproc remoteproc1: Booting fw image j7-c66_1-fw, size 144652
[    7.450066] PVR_K:  210: Read BVNC 22.104.208.318 from HW device registers
[    7.457091] virtio_rpmsg_bus virtio0: creating channel ti.ipc4.ping-pong addr 0xd
[    7.466070] virtio_rpmsg_bus virtio0: creating channel rpmsg_chrdev addr 0xe
[    7.476058] img_enc 4200000.video-encoder: vxe_enc_probe: using heap 1 for internal alloc
[    7.489691] k3-dsp-rproc 4d81800000.dsp: booting DSP core using boot addr = 0xa7200400
[    7.504106]  remoteproc1#vdev0buffer: assigned reserved memory node c66-dma-memory@a6000000
[    7.516372] virtio_rpmsg_bus virtio1: rpmsg host is online
[    7.529257]  remoteproc1#vdev0buffer: registered virtio1 (type 7)
[    7.541537] remoteproc remoteproc1: remote processor 4d81800000.dsp is now up
[    7.555117] virtio_rpmsg_bus virtio1: creating channel ti.ipc4.ping-pong addr 0xd
[    7.566572] virtio_rpmsg_bus virtio1: creating channel rpmsg_chrdev addr 0xe
[    7.572031] remoteproc remoteproc2: 64800000.dsp is available
[    7.577922] platform 41000000.r5f: R5F core may have been powered on by a different host, programmed state (0) != actual state (1)
[    7.587977] PVR_K:  210: RGX Device registered with BVNC 22.104.208.318
[    7.604152] [drm] Initialized tidss 1.0.0 20180215 for 4a00000.dss on minor 1
[    7.612564] tidss 4a00000.dss: [drm] Cannot find any crtc or sizes
[    7.614404] img_enc 4200000.video-encoder: encoder registered as /dev/video0
[    7.623744] tidss 4a00000.dss: [drm] Cannot find any crtc or sizes
[    7.627174] img_dec 4300000.video-decoder: decoder registered as /dev/video1
[    7.636385] [drm] Initialized pvr 1.15.6133109 20170530 for 4e20000000.gpu on minor 0
[    7.654906] platform 41000000.r5f: configured R5F for IPC-only mode
[    7.662055] platform 41000000.r5f: assigned reserved memory node r5f-dma-memory@a0000000
[    7.689116] remoteproc remoteproc3: 41000000.r5f is available
[    7.700498] remoteproc remoteproc3: attaching to 41000000.r5f
[    7.707137] platform 41000000.r5f: R5F core initialized in IPC-only mode
[    7.717466]  remoteproc3#vdev0buffer: assigned reserved memory node r5f-dma-memory@a0000000
[    7.729101] virtio_rpmsg_bus virtio2: rpmsg host is online
[    7.735311]  remoteproc3#vdev0buffer: registered virtio2 (type 7)
[    7.742204] remoteproc remoteproc3: remote processor 41000000.r5f is now attached
[    7.753363] platform 5c00000.r5f: configured R5F for remoteproc mode
[    7.762076] platform 5c00000.r5f: assigned reserved memory node r5f-dma-memory@a2000000
[    7.771815] remoteproc remoteproc4: 5c00000.r5f is available
[    7.781140] platform 5d00000.r5f: configured R5F for remoteproc mode
[    7.790314] platform 5d00000.r5f: assigned reserved memory node r5f-dma-memory@a3000000
[    7.800918] remoteproc remoteproc5: 5d00000.r5f is available
[    7.810211] platform 5e00000.r5f: configured R5F for remoteproc mode
[    7.819211] platform 5e00000.r5f: assigned reserved memory node r5f-dma-memory@a4000000
[    7.832723] remoteproc remoteproc6: 5e00000.r5f is available
[    7.844449] platform 5f00000.r5f: configured R5F for remoteproc mode
[    7.864463] platform 5f00000.r5f: assigned reserved memory node r5f-dma-memory@a5000000
[    7.872633] remoteproc remoteproc5: powering up 5d00000.r5f
[    7.878227] remoteproc remoteproc5: Booting fw image j7-main-r5f0_1-fw, size 98828
[    7.880749] remoteproc remoteproc7: 5f00000.r5f is available

The SDK we used is 08.06.00.12.

Could you give us some advices?

Best Regards,

Zhang