Hi,
We have discovered an issue here. Firstly, we set the "enable_error_detection" in "app_multi_cam_codec. cfg" to 1.
1. We connect four cameras and configure four cameras when running the program.
If a camera is unplugged during operation (if a third camera is unplugged), the error_frame can be presented normally.
2. However, if we unplug one camera before running the program (taking the third camera as an example), the number of cameras configured when running the program will still be 4.
However, during runtime, all four screens will display incorrect frames of images, which will cause the other three cameras to also be unable to produce images properly.
sdk:08.06.00.12 app_multi_cam_codec
Regards,
Yueqian