This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM368 Changing Sensor Mode Problem (H3A)

Hi,

 

I am currently working on a product using DM368 with Micron MT9T001 3M pixel sensor. The specification of the product supports two output modes which are sensor full-size and binning mode. However, while changing between the two modes, it may occur a situation that the H3a return an abnormal AEWB statistics data, being fixed values which is not responding the input signal from sensor. The situation causes the following AEWB algorithm malfunctioning. Does anyone have met any similar situation before?

 

Cheers

 

Jeff