Part Number: PROCESSOR-SDK-AM64X
Hi
May I have question about processor-sdk's U-boot?
I used u-boot-spl/bl31/bl32 prebuilt image for make linux.appimage.
And boot from eMMC.
So I shoud change U-boot environment variable (ex. mmcdev/bootpart) from U-boot.
But I cannot use "saveenv" command, So I can not save and must change environment variables each time the processor booting.
Is there any way to enable "saveenv" command?
Or Is there any way to change environment variable from u-boot?

--
full log
・MSC Firmware Version 9.1.6--v09.01.06 (Kool Koala)
DMSC Firmware revision 0x9
DMSC ABI revision 3.1
[BOOTLOADER_PROFILE] Boot Media : undefined
[BOOTLOADER_PROFILE] Boot Image Size : 0 KB
[BOOTLOADER_PROFILE] Cores present :
[BOOTLOADER PROFILE] System_init : 12396us
[BOOTLOADER PROFILE] Drivers_open : 55499us
[BOOTLOADER PROFILE] Board_driversOpen : 0us
[BOOTLOADER PROFILE] App_loadImages : 61634us
[BOOTLOADER_PROFILE] SBL Total Time Taken : 290445us
Image loading done, switching to application ...
Starting linux and RTOS/Baremetal applications
NOTICE: BL31: v2.9(release):v2.9.0-614-gd7a7135d32-dirty
NOTICE: BL31: Built : 09:34:15, Aug 24 2023
I/TC:
I/TC: OP-TEE version: 4.0.0 (gcc version 11.4.0 (GCC)) #1 Fri Oct 20 18:29:31 UTC 2023 aarch64
I/TC: WARNING: This OPE-TEER confiRguraOtion Rmig:ht be Binsoecure!
I/TC: WARNING: Please check https://optee.readthedocs.io/en/latest/architecture/porting_guidelines.html
I/TC: Primary CPU initializing
I/TC: SYSFW ABI: 3.1 (firmware rev 0x0009 '9.1.6--v09.01.06 (Kool Koala)')
I/TC: HUK Initialized
I/TC: Activated SA2UL device
I/TC: Enabled firewalls for SA2UL TRNG device
I/TC: SA2UL TRNG initialized
I/TC: SA2UL Drivers initialized
I/TC: Primary CPU switching to normal world boot
U-Boot SPL 2023.04-gb0d717b732 (Dec 06 2023 - 15:11:45 +0000)
SYSFW ABI: 3.1 (firmware rev 0x0009 '9.1.6--v09.01.06 (Kool Koala)')
Trying to boot from MMC1
Authentication passed
Authentication passed
U-Boot 2023.04-gb0d717b732 (Dec 06 2023 - 15:11:45 +0000)
SoC: AM64X SR2.0 HS-FS
Model: Texas Instruments AM642 EVM
Board: AM64-EVM rev C
DRAM: 2 GiB
Core: 66 devices, 31 uclasses, devicetree: separate
NAND: 0 MiB
MMC: mmc@fa10000: 0, mmc@fa00000: 1
Loading Environment from nowhere... OK
In: serial@2800000
Out: serial@2800000
Err: serial@2800000
Unidentified board claims AM64-EVM in eeprom header
Net: eth0: ethernet@8000000port@1
Hit any key to stop autoboot: 0
=> setenv mmcdev 0
=> setenv bootpart 0:1
=> saveenv
Unknown command 'saveenv' - try 'help'
=> env save
env - environment handling commands
Usage:
env ask name [message] [size] - ask for environment variable
env default [-f] -a - [forcibly] reset default environment
env default [-f] var [...] - [forcibly] reset variable(s) to their default values
env delete [-f] var [...] - [forcibly] delete variable(s)
env edit name - edit environment variable
env exists name - tests for existence of variable
env export [-t | -b | -c] [-s size] addr [var ...] - export environment
env import [-d] [-t [-r] | -b | -c] addr [size] [var ...] - import environment
env print [-a | name ...] - print environment
env run var [...] - run commands in an environment variable
env set [-f] name [arg ...]
=> <INTERRUPT>
=>
Thanks,
GR