This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SK-AM64B: Ethernet/IP communication implementation

Part Number: SK-AM64B

  1. I want to use the SK-AM64B board for communication in the Ethernet/IP network. Assuming that the RF5 core is used to communication with Ethernet/IP protocol, is there any example showing the ability to read/write parameters sending between devices over Ethernet/IP from RT-Linux (A53 core). Maybe there is a dedicated module for this purpose on Linux?
  1. How to define communication objects for ethernet/ip in PRU module?
  2. Moreover I would like to use Ethernet ports simultaneously for Ethernet/IP and for web page hosted on Linux. Are Ethernet ports managed by PRU-ICSS visible on Linux(A53 core) like standard Ethernet ports?