This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: SBL

Part Number: TDA4VM

[FAQ] TDA4VM: Run vision_apps in SBL boot flow with combined_appImage

Referring to the reply in the previous post, when the SD card is started, the serial port output of the MCU is as follows:

SBL Revision: 01.00.10.01 (Jan 15 2024 - 15:22:24)
TIFS  ver: 9.1.2--v09.01.02 (Kool Koala)

There are no other prints left behind.