Other Parts Discussed in Thread: UCD9222
I have a couple of questions regarding the Smart Reflex power circuit used on the TMDXEVM6678L eval board…
1. The four VID2 pins of the UCD9222 device are connected to the FPGA. I believe these pins are used to control the dynamic voltage on the associate rail. Since the voltage on Rail#2 is fixed, rather than dynamic, what is the FPGA doing with these pins?
a. Do these pins need to be connected if there is no need for a dynamic voltage on Rail#2 of the UCD9222 device?
b. If they do not need to be connected, how should they be terminated?
2. The PMBus of the UCD9222 device is connected to the FPGA, as well as to a test header. Does the bus need to be connected to another device for some reason, or is a header sufficient?
3. According to the EN1/EN2 description in the UCD9222 datasheet, “When the ON_OFF_CONFIG setting is configured to respond the PMBus_Cntrl pin, the PMBus_Cntrl pin signal will be logically ANDed withthe rail’s EN pin signal.” I assume that all ON_OFF_CONFIG options (not just the PMBust_Cntrl pin option) will be logically ANDed with the rail's EN pin signal, so that no matter what setting is selected the EN signal must be asserted in order for the rail to turn on. For example, if the ON_OFF_CONFIG command were such that the rails were set to turn on automatically, they would not turn on until the enable signals were asserted. Can you please confirm this?
Thank you very much for you help.