Other Parts Discussed in Thread: DM3730
I am designing a schematic with the DM3730 DSP. I may need to connect two cameras to my board. I see in the specifications that this is possible utilizing SCCB (serial camera control bus) on the I2C ports. I see a max data rate of 100kbits/s for the SCCB interface protocol. Is that accurate?
I am trying to figure out how far away I can have my camera from by board. I am looking to place one camera with one foot but the 2nd camera would be roughly 25ft away. Is this possible?