Hi,
I would like to ask about the ability of OMAP L138's LCD display.

As SPRUGJ9B TMS320C674x_OMAP-L1x Processor Video Port Interface (VPIF) User's Guide show, there are two input and two output channels within VPIF. The question is on how they are integrated with LCD controller?
I am comparing two devices: DM6437 and OMAP L138. DM6437 has a powerful VPSS which consists of VPFE and VPBE, and these two forms a front-back ends pair that is closely integrated, so there is no problem for VPFE's video stream to get displayed through VPBE, and they could be well synchronized.
For OMAP L138, according to SPRUGJ9B it supports BT.656 stream input video, but could this video get displayed on a backend LCD through LCDC output?
Further, normally LCD requires frame rate of over 75Hz, however standard NTSC video consists of only 30 frames or 60 interlaced fields per second. There is no integer multiplication relationship between 75 and 30/60, so how does the synchronization works if LCD can be made to display BT.656 stream?
Zheng