This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I'm working on TDA4VH with sdk0900, and I want to use DMA to transfer data.
But, when I use DMA to transfer data to the DDR obtained from the system memory, c7x gets stuck.
The current data size to transfer is 83072 bytes.
I use the following interface to obtain DDR memory:
I have obtained a total of 498432 bytes of DDR space.
Hi Team,
customer report this issue when he develops TIDL custom layer.
Hi Jinsong,
can you help upload more error log or more information for TI expert further analysis?
BR,
Biao
Hi,
I am sorry i could not understand the above code, could you please share the code? Or is this available somewhere in the SDK?
Regards,
Brijesh