This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6748 Silicon Revision 2.0 EDMA3CC REVID & NUM_DMACH

Hi,

My customer read the REVID register and CCCFG.NUM_DMACH bit field of EDMA3CC of C6748 rev 2.0, then confirmed the values were 4001_9B00h and 4h respectively.

But, acording to the EDMA3 UG (SPRUGP9B), the REVID is 4001_5300h and the CCCFG.NUM_DMACH is Reserved.
Which values are correct?

Thanks in advance for your cooperation.

Best regards,
j-breeze