This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Firmware file loading problem



Hi,

I am working with DM365 custom board the linux kernel version is 2.6.37.

I am working with a codec which requires firmware to be loaded. I have placed the firmware file in the path.

"usr/lib/firmware" it is not working, i am getting the error.

codec_download_firmware(): Firmware codec.fw not available -2
codec_init: failed to download firmware

error -2 indicates file not available. I think the path is not correct, can you please suggest which path i should place the firmware file and also any configuration i need to enable in the kernel.

Thank you.