This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SK-AM62: SK-Am62x E3 USB-DFU method to load custom image to EMMC

Part Number: SK-AM62

If we have to load the custom image to the EMMC using usb-dfu method what have to be done .

i tried loading the default image also but it shows size issue at the below point

"tisdk-default-image-am62xx-evm.tar.xz"

$ sudo dfu-util -a rootfs -D tisdk-base.ext4
dfu-util 0.9

Copyright 2005-2009 Weston Schmidt, Harald Welte and OpenMoko Inc.
Copyright 2010-2016 Tormod Volden and Stefan Schmidt
This program is Free Software and has ABSOLUTELY NO WARRANTY
Please report bugs to sourceforge.net/.../

dfu-util: File size is too big: Success

The default image is actually of 5.4gb

Also want to know how the memory is allocated for this in EMMC (also need to know how to edit the size)