Hello TI experts,
It's about the Pin L18 VMON6_IR_VEXT0P8 of TDA4AL, the threshold is only 0.8V while the supply of VDD_CORE or VDD_MCU is 0.8V too.
So how does the VMON6_IR_VEXT0P8 monitor VDD_CORE or VDD_MCU?
Thanks a lot.


This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello TI experts,
It's about the Pin L18 VMON6_IR_VEXT0P8 of TDA4AL, the threshold is only 0.8V while the supply of VDD_CORE or VDD_MCU is 0.8V too.
So how does the VMON6_IR_VEXT0P8 monitor VDD_CORE or VDD_MCU?
Thanks a lot.


Huan,
You can get a pretty good understanding of this through the TRM section 5.2.3.1. The voltage levels are set by CTRL_MMR_POK_VDD_CPU1_UV_CTRL and CTRL_MMR_POK_VDD_CPU1_OV_CTRL. The 0P8 nomenclature on the pin is intended to tell you that the voltage range is 0.8V (rather than 1.8V or 3.3V).
Kevin