This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDS64GPEVM: PROCESSOR-SDK-AM64X

Part Number: TMDS64GPEVM

Hi , 

I am working on AM64x-evm 

I want to use I2C-0 on the board to read the data from EEPROM for that I have to select/muxed in device tree, for that i have added the block in device tree

 

&main_pmx0 {
	main_i2c0_pins_default: main-i2c0-pins-default {
		pinctrl-single,pins = <
			AM64X_IOPAD(0x0260, PIN_INPUT_PULLUP, 0) /* (A18) I2C0_SCL */
			AM64X_IOPAD(0x0264, PIN_INPUT_PULLUP, 0) /* (B18) I2C0_SDA */
		>;
	};
};

&main_i2c0 {
	pinctrl-names = "default";
	pinctrl-0 = <&main_i2c0_pins_default>;
	clock-frequency = <100000>;
};

now I want to compile and proceed further to build and image and enable the I2C-0 node . I tried the command 

make ARCH=arm64 CROSS_COMPILE=aarch64-none-linux-gnu- ti/k3-am642-evm.dtb 

but it is not working.